Part Number: PROCESSOR-SDK-C6748
Other Parts Discussed in Thread: OMAPL138, CCSTUDIO
Tool/software: Code Composer Studio
2. Install processor SDK RTOS for OMAPL138, selecting C6000 support
3. Run CCS to register components installed in step 2
4. In processor_sdk_rtos_omapl138_5_03_00_07 directory, run setupenv.bat/sh, then (g)make
5. In pdk_omapl138_1_0_8\packages directory, run/source pdsetupenv.bat/sh, then (g)make
6. In pdk_omapl138_1_0_8\packages directory, run pdkProjectCreate.bat/sh with arguments "C6748 all little all example dsp"
On Windows, I get <pastebin.com/K3yrsAPg>. On Linux, I get <pastebin.com/74Rj5i47>. Both platforms are failing to find something. On Linux it helped to manually create the MyExampleProjects directory. I didn't notice any errors earlier in the process.
Any ideas why this is failing? We really need the MCASP example for C6748 to get started with development and catch up to competitors we're also evaluating.