This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: TDA2Px

Part Number: TDA2P-ACD
Other Parts Discussed in Thread: DS90UH949-Q1, DS90UH928Q-Q1

We need your help on the below query.

 

Our processor side(TDA2Px), HDMI interface is aligned with the HDMI TMDS single stream standard v1.4a (720p

@60Hz to 1080p @24Hz) and the HDMI v1.3 (1080p @60Hz): 3 data channels, plus 1 clock channel is

supported (differential).

 

In DS90UH949-Q1 serializer(On SoC side), Supports TMDS clock up to 170 MHz for WUXGA (1920x1200) and 1080p60 resolutions with 24-bit color depth

 

In DS90UH928Q-Q1 deserializer(On Display side), Supports High Definition (720p) Digital Video

 

In Case of displays, the resolution we considered are 800 x 600(low cost) and 1,024×(B,G,R)(W)×768(H)(high cost).

 

Can we able to use these two displays(Low cost/high cost) with different resolution in this serializer/desrializer configuration.

 

While we looking in resolution perspective, SoC, serializer/deserializer, Display resolutions are different.

Please let me know this resolution mismatch affects any proper device functionality/quality?