Hi, all,
I'm trying to connect a custom lcd rgb565 display to the dc5 connector of dm355.
The boot params in the u-boot env include "davinci_enc_mngr.ch0_output=LCD davinci_enc_mngr.ch0_mode=640x480"
I can see the LCD_OE, HSYNC, VSYNC signals and 27MHz VCLK on the osciloscope, but there are no signals on the video data output pins.
I'm using dvsdk_2_00_00_18, montavista 5.0 and kernel linux-2.6.18_pro500.
I would be very thankful if someone can help me to make this display work.
Thanks in advance
Hristo Tsenov
AsisBG - Varna