This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM65X: Android SD card create issue

Part Number: PROCESSOR-SDK-AM65X

Tool/software: Linux

Hi, 

I am using AM65x EVM and trying to boot Android from SD card.

I've followed all the steps given on the website. I think there is some problem with  create-sdcard.sh provided with the SDK ti-processor-sdk-android-am65xx-evm-05.03.00.07-Linux-x86-Install.bin

 


In the script, there is support for only 5 binaries:

0. BOOTFILEPATH

1. BOOTIMG

2. BOOTUENV

3. SPL_A53

4. SPL_R5

5. SYSFW

That's all!

There is no support for KERNELIMAGE, RAMDISKIMG, SYSTEMIMG, USERDATAIMG etc.

Kindly, review the create-sdcard.sh script which is uploaded on the following TI link:

http://software-dl.ti.com/processor-sdk-android/esd/AM65X/latest/index_FDS.html

Thanks,

Tarun