Other Parts Discussed in Thread: TMS320DM355
Hi,
I turned on the TMS320DM355 DVEVM board for the first time. The video demo never come up on the screen (TV-out). The last few lines on the UART is shown below.
Please give me some hints to get it going.
Thanks,
Pho Hoang
Hash tables configured (established 8192 bind 16384)
Initializing XFRM netlink socket
NET: Registered protocol family 1
NET: Registered protocol family 10
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
yaffs: dev is 32505859 name is "mtdblock3"
yaffs: Attempting MTD mount on 31.3, "mtdblock3"
block 109 is bad
block 715 is bad
block 1459 is bad
block 2224 is bad
block 2225 is bad
block 2337 is bad
block 2763 is bad
block 4003 is bad
VFS: Mounted root (yaffs2 filesystem).
Freeing init memory: 180K
ioremap_nocache(0x87400000, 12582912)=0xc7880000
allocated heap buffer 0xc7880000 of size 0xce000
cmem initialized 8 pools between 0x87400000 and 0x88000000