Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hi,
I am trying to create project files for ethernet Ip adapter for am335x.
But I am getting this error
test@lpz-jags-3:/u/EIP/protocols/ethernetip_adapter/projects$ sudo ./projectCreate.sh AM335x arm ethernetip_adapter
**************************************************************************
Environment Configuration Summary:
CCS Install Directory : /u/ti/ccsv6/
CCS Workspace Directory : /tmp/ccs_workspace
SDK Install Directory : /u/EIP
PDK Install Directory : /u/ti-processor-sdk-linux-am335x-evm-05.03.00.07
Projects create Directory : /u/EIP/protocols/ethernetip_adapter/projects
Project create args directory : /u/EIP/protocols/ethernetip_adapter/projects/ccsproject_args
**************************************************************************
Creating project 'ethernetip_adapter_AM335x_arm' for 'AM335x' platform in directory '/u/EIP/protocols/ethernetip_adapter/projects/ethernetip_adapter_AM335x_arm' by overwriting the project if it exists already...
--------------------------------------------------------------------------------
Creating project 'ethernetip_adapter_AM335x_arm'...
!ERROR: Compiler version 'GNU_6.3.1:Linaro' is not currently installed!
test@lpz-jags-3:/u/EIP/protocols/ethernetip_adapter/projects$ arm-linux-gnueabihf-gcc --version
arm-linux-gnueabihf-gcc (Linaro GCC 7.2-2017.11) 7.2.1 20171011
Copyright (C) 2017 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
test@lpz-jags-3:/u/EIP/protocols/ethernetip_adapter/projects$
Linaro I am installed is 7.2, But it is not taking it.
Thanks and Regrads,
Vishnu