Part Number: AM4379
Other Parts Discussed in Thread: TIDA-010016, PROFIBUS
Tool/software: TI-RTOS
Hi folks,
I have the EtherCAT_Slave_full_AM437x_arm Demo running on my idk4379 board with a custom ESI-file.
I also have achieved to get the IO-LINK Master Demo running with hardware like TIDA-010016.
Now i want to combine Both of these Demos to have IO-Link Data on EtherCAT available running one Part on PRU0 and the other part on PRU1.
1. So which hardware changes on idkAM4379 i have to do to archieve this ?
2. Also how can i get both of these demos running one on PRU1 and other on PRU0 ?
3. How to intercommunicate between these two PRU's
thx in advance
Haxor