Part Number: TDA3XEVM
Tool/software: TI-RTOS
Hello.
For a long time I worked with VSDK305 and after the release of VSDK307 I found MPEG4 Encode link in release notes, which is interesting for me. I want to add it to a current VSDK305 project, because moving the whole project to VSDK307 seems not worth it for now.
I have successfully added link to VSDK305 and created a usecase, but appimage with it crushes right at the moment of MPEG4 plugin initialization on DSP.
What should I change to make it start working? I added mem_segment_definition_512mb.xs from VSDK307 to VSDK305 , because i think that some kind of memory problem causes the crashes, but i didn't see any differences. Should I also add the ti-cgt-c6000_8.2.4 compiler from VSDK307 or smth else?