This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/DRA745: run rtos error: Jumping to MPU CPU0 App

Part Number: DRA745

Tool/software: TI-RTOS

Jumping to MPU CPU0 App

TDA2xx SBL Boot

DPLL Configuration Completed

Clock Domain Configuration Completed

Module Enable Configuration Completed

TI EVM PAD Config Completed

DDR Config Completed

App Image Download Begins

SD Boot - file open completed successfully

MPU CPU0 Image Load Completed

IPU1 CPU1 Image Load Completed

IPU2 CPU0 and CPU1 Image Load Completed

DSP1 Image Load Completed

DSP2 Image Load Completed

EVE1 Image Load Completed

EVE2 Image Load Completed

EVE3 Image Load Completed

EVE4 Image Load Completed

App Image Download Completed

Putting MPU CPU1 in Off mode

EVE MMU configuration completed

EVE MMU configuration completed

EVE MMU configuration completed

EVE MMU configuration completed

*****************************************************************

PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles

SBL Initial Config Cycles - 144553 (12.33 ms)
SOC Init Cycles - 164782 (14.6 ms)
DDR Config Clock Cycles - 43438 (3.70 ms)
App Image Load Cycles - 231177367 (19727.13 ms)
Slave Core Bootup Cycles - 208367 (17.78 ms)
SBL Boot-up Cycles - 231739570 (19775.10 ms)
Time at which SBL started IPU1_0 - 7072608 (603.52 ms)
*****************************************************************

Jumping to MPU CPU0 App

It stop here. could you give some comments ? thanks.

  • Hi,

    There could be various causes of this issue.

    What are the changes have you made?

    First try to find out which core is causing this.

    Try first by enabling only IPU1_0 and check and keep on adding 1 core at a time and check.

    You need to connect CCS and check where exactly it is stuck.?

    Regards,

    Anuj

  • Hi,

    Its been long since any update on this thread.

    I hope you are able to resolve your issue.

    If not then please reply below or create a new thread for some different query.

    Regards,

    Anuj