Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
Tool/software: Code Composer Studio
Hello,
Im using the IWR1443 Boost radar sensor togehter with TSW1400_board and the mmWave DevPack to capture the raw data.
Now I want to set my duty Cycle in the Radar Studio GUI to 100%. So that I have a countinous stream(lets say 2.5 seconds) of Chirps with out interleaving time between the frames.
For example with following Settings
Slope=25.009e12
adcSamples=256
tChirp=80e-6
tIdle=10e-6
period=11.52e-3
noFrames=250
noChirps=128
I tried this settings but i cant start my measurment.
Now my question is. Is it possible to set the Duty Cyle to 100% ?
Best regards,
Patrick