Part Number: AM3352
Tool/software: Linux
Hi champs
I know in the TRM it indicates that SYSBOOT pins [11:6] are dont care if we use boot mode 11100b. What i am worried about is that in all the TI platforms we pull all the sysboot pins either high or low no matter what boot mode we use. So i am trying to double check to make sure that those sysboot pins can be left floating.
Also if i use pins U1 and U2 for uart2 CTS and RTS do i have to pull them high or low because they are used as sysboot pins when the processor boots? I know that the sysboot pins are read on the rising edge of the reset but if these are don't care then it should not matter correct?
We are seeing some strange behavior from a customer board and trying to see what can cause the strange behavior.
Thanks
Regards
Mohsen