Part Number: 66AK2E05
Other Parts Discussed in Thread: DA8XX
Tool/software: Linux
Hi community,
Im working on Keystone K2E EVM. I downloaded Processor-SDK-Linux-RT-K2E. I want to run one Core Linux with a custom configuration, but i failed. I get these 2 errors:
Internal error: Oops: 206 [#1] PREEMPT SMP ARM
Kernel Panic (Unable to handle kernel paging request at virtual address)
Im using a custom uboot, there is no bootargs available in uboot environment in this uboot configuration. When i use prebuild-images, i see only "Uncompressing Linux... done, booting the kernel.". I think kernel hangs on booting, but i cant see where because of bootargs not available(therefore no earlyprintk available too). So i recompiled linux kernel.
I want to create a zImage completely undepended from uboot, bootargs etc. So, i changed this rows inside 'arch/arm/configs/tisdk_k2e-evm-rt_defconfig' to;
# CONFIG_CMDLINE_PARTITION is not set
# CONFIG_ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER is not set
# CONFIG_MTD_CMDLINE_PARTS is not set
# CONFIG_FB_CMDLINE is not set
CONFIG_CMDLINE="console=ttyS0,115200n8 rootwait=1 earlyprintk root=/dev/ram0 rw"
# CONFIG_BLK_CMDLINE_PARSER is not set
CONFIG_TTY_PRINTK=y
CONFIG_CMA_SIZE_MBYTES=192
CONFIG_PAGE_OFFSET=0xD0000000
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_NR_CPUS=1 for One Core Linux
And
all **_DEBUG_** lines set to '=y'
I want to remap footprint from default(0x80000000-0xC0000000) to (0xD0000000-0xF8000000). So i changed
'arch/arm/boot/dts/keystone.dtsi' inside;
'memory {reg = <0x00000000 0xD0000000 0x00000000 0x28000000>;};'
' soc {...; ranges = <0x0 0x0 0x0 0xFFFFFFFF>; dma-ranges = <0xD0000000 0x8 0x00000000 0x28000000>; ...}'
'arch/arm/boot/dts/keystone-k2e.dtsi' inside;
remove cpu@1, cpu@2, cpu@3 for Once Core Linux
'arch/arm/Kconfig' inside;
PAGE_OFFSET 0x80000000 to 0xD0000000
With above configuration(conf1), kernel hangs on boot. I think i missed some address configuration for remapping. Here is the output;
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.79-rt47-ga72bf1418c (srt@ubuntu) (gcc version 7.4.0 (Ubuntu/Linaro 7.4.0-1ubuntu1~18.04.1)) #1 SMP PREEMPT RT Tue Jul 9 05:43:17 PDT 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: Texas Instruments Keystone 2 Edison EVM
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at arch/arm/mm/physaddr.c:42 __virt_to_phys+0xc4/0xc8
[ 0.000000] virt_to_phys used for non-linear address: f0000000 (0xf0000000)
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 4.14.79-rt47-ga72bf1418c #1
[ 0.000000] Hardware name: Keystone
[ 0.000000] Backtrace:
[ 0.000000] [<d020c4f4>] (dump_backtrace) from [<d020c7d8>] (show_stack+0x18/0x1c)
[ 0.000000] r7:600001d3 r6:d106aa44 r5:00000000 r4:d106aa44
[ 0.000000] [<d020c7c0>] (show_stack) from [<d09a65f0>] (dump_stack+0x80/0x94)
[ 0.000000] [<d09a6570>] (dump_stack) from [<d021fe00>] (__warn+0xec/0x104)
[ 0.000000] r7:00000009 r6:d0bbbcf0 r5:00000000 r4:d1001e68
[ 0.000000] [<d021fd14>] (__warn) from [<d021fe58>] (warn_slowpath_fmt+0x40/0x48)
[ 0.000000] r9:00000000 r8:ffffffff r7:00000000 r6:7fffffff r5:d0e46278 r4:d0bbbcb8
[ 0.000000] [<d021fe1c>] (warn_slowpath_fmt) from [<d0218a3c>] (__virt_to_phys+0xc4/0xc8)
[ 0.000000] r3:f0000000 r2:d0bbbcb8
[ 0.000000] r4:f0000000
[ 0.000000] [<d0218978>] (__virt_to_phys) from [<d0e2da0c>] (early_init_fdt_reserve_self+0x28/0x4c)
[ 0.000000] r9:d1014ac0 r8:d1083e88 r7:d1001fc4 r6:d1083e8c r4:d1a6f4c8
[ 0.000000] [<d0e2d9e4>] (early_init_fdt_reserve_self) from [<d0e06a58>] (arm_memblock_init+0x174/0x1b8)
[ 0.000000] r4:d0200000
[ 0.000000] [<d0e068e4>] (arm_memblock_init) from [<d0e04628>] (setup_arch+0x5f0/0xbf8)
[ 0.000000] r10:d1083f80 r9:d1014ac0 r8:d0e45a48 r7:d1001fc4 r6:d0008000 r5:d0e3d270
[ 0.000000] r4:d1a79148
[ 0.000000] [<d0e04038>] (setup_arch) from [<d0e00a3c>] (start_kernel+0x68/0x404)
[ 0.000000] r10:00000000 r9:412fc0f4 r8:d100fe80 r7:d1014c38 r6:00000000 r5:d100fe98
[ 0.000000] r4:00000000
[ 0.000000] [<d0e009d4>] (start_kernel) from [<d0008090>] (0xd0008090)
[ 0.000000] r10:00000000 r9:412fc0f4 r8:d0007000 r7:d1014c38 r6:d0e45a44 r5:d100fe98
[ 0.000000] r4:d10840d4
[ 0.000000] ---[ end trace 0000000000000001 ]---
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000081f800000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node dsp-common-memory@81f800000, compatible id shared-dma-pool
[ 0.000000] cma: dma_contiguous_reserve(limit 4fffffff)
[ 0.000000] cma: dma_contiguous_reserve: reserving 192 MiB for global area
[ 0.000000] cma: cma_declare_contiguous(size 0x000000000c000000, base 0x0000000000000000, limit 0x000000014fffffff alignment 0x0000000000000000)
[ 0.000000] cma: Reserved 192 MiB at 0x00000000e4000000
[ 0.000000] On node 0 totalpages: 163840
[ 0.000000] free_area_init_node: node 0, pgdat d106ac40, node_mem_map e39f8000
[ 0.000000] DMA zone: 1152 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 131072 pages, LIFO batch:31
[ 0.000000] HighMem zone: 32768 pages, LIFO batch:7
[ 0.000000] Unable to handle kernel paging request at virtual address f0000000
[ 0.000000] pgd = d0003000
[ 0.000000] [f0000000] *pgd=800000d0007003, *pmd=00000000
[ 0.000000] Internal error: Oops: 206 [#1] PREEMPT SMP ARM
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Tainted: G W 4.14.79-rt47-ga72bf1418c #1
[ 0.000000] Hardware name: Keystone
[ 0.000000] task: d1012d80 task.stack: d1000000
[ 0.000000] PC is at fdt_check_header+0xc/0x80
[ 0.000000] LR is at __unflatten_device_tree+0x74/0x2b0
[ 0.000000] pc : [<d09a67ac>] lr : [<d07ec7b8>] psr: 600000d3
[ 0.000000] sp : d1001ec0 ip : d1001ed0 fp : d1001ecc
[ 0.000000] r10: 00000000 r9 : d1a6f4b0 r8 : 00000000
[ 0.000000] r7 : d0e2c9c4 r6 : f0000000 r5 : d0e3d270 r4 : d1077460
[ 0.000000] r3 : 00000000 r2 : d1a6f4b0 r1 : 00000000 r0 : f0000000
[ 0.000000] Flags: nZCv IRQs off FIQs off Mode SVC_32 ISA ARM Segment user
[ 0.000000] Control: 30c5387d Table: d0003000 DAC: fffffffd
[ 0.000000] Process swapper (pid: 0, stack limit = 0xd1000210)
[ 0.000000] Stack: (0xd1001ec0 to 0xd1002000)
[ 0.000000] 1ec0: d1001efc d1001ed0 d07ec7b8 d09a67ac d0e2c9c4 d0e2c9c4 d0e3d270 d1599520
[ 0.000000] 1ee0: d0000000 00000000 d1014ac0 d1083f80 d1001f1c d1001f00 d0e2db2c d07ec750
[ 0.000000] 1f00: 00000000 d1001f10 d0227638 d1012a40 d1001fa4 d1001f20 d0e049b0 d0e2dafc
[ 0.000000] 1f20: 00000000 00000000 00000000 00000000 ffffffff d1001f40 d027f080 d0e3d270
[ 0.000000] 1f40: fffff000 d1024020 00000000 f7ffffff d0280544 d027f064 d0000000 00000000
[ 0.000000] 1f60: 00000000 d100fe98 00000000 d1014c38 d1001f94 d1001f80 d027fce8 00000000
[ 0.000000] 1f80: d100fe98 00000000 d1014c38 d100fe80 412fc0f4 00000000 d1001ff4 d1001fa8
[ 0.000000] 1fa0: d0e00a3c d0e04044 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.000000] 1fc0: 00000000 d0e45a48 00000000 d10840d4 d100fe98 d0e45a44 d1014c38 d0007000
[ 0.000000] 1fe0: 412fc0f4 00000000 00000000 d1001ff8 d0008090 d0e009e0 00000000 00000000
[ 0.000000] Backtrace:
[ 0.000000] [<d09a67a0>] (fdt_check_header) from [<d07ec7b8>] (__unflatten_device_tree+0x74/0x2b0)
[ 0.000000] [<d07ec744>] (__unflatten_device_tree) from [<d0e2db2c>] (unflatten_device_tree+0x3c/0x4c)
[ 0.000000] r10:d1083f80 r9:d1014ac0 r8:00000000 r7:d0000000 r6:d1599520 r5:d0e3d270
[ 0.000000] r4:d0e2c9c4 r3:d0e2c9c4
[ 0.000000] [<d0e2daf0>] (unflatten_device_tree) from [<d0e049b0>] (setup_arch+0x978/0xbf8)
[ 0.000000] r4:d1012a40
[ 0.000000] [<d0e04038>] (setup_arch) from [<d0e00a3c>] (start_kernel+0x68/0x404)
[ 0.000000] r10:00000000 r9:412fc0f4 r8:d100fe80 r7:d1014c38 r6:00000000 r5:d100fe98
[ 0.000000] r4:00000000
[ 0.000000] [<d0e009d4>] (start_kernel) from [<d0008090>] (0xd0008090)
[ 0.000000] r10:00000000 r9:412fc0f4 r8:d0007000 r7:d1014c38 r6:d0e45a44 r5:d100fe98
[ 0.000000] r4:d10840d4
[ 0.000000] Code: e89da800 e1a0c00d e92dd800 e24cb004 (e5903000)
[ 0.000000] ---[ end trace 0000000000000002 ]---
[ 0.000000] Kernel panic - not syncing: Attempted to kill the idle task!
When i changed footprint back from (0xD0000000-0xF8000000) to (0x80000000-0xFFFFFFFF)
'arch/arm/boot/dts/keystone.dtsi' inside;
'memory {reg = <0x00000000 0x80000000 0x00000000 0x80000000>;};'
' soc {...; ranges = <0x0 0x0 0x0 0xFFFFFFFF>; dma-ranges = <0x80000000 0x8 0x00000000 0x80000000>; ...}'
With (0x80000000-0xFFFFFFFF) mapping configuration(conf2), Kernel hangs on a little bit forward stage. Here is the output;
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.79-rt47-ga72bf1418c (srt@ubuntu) (gcc version 7.4.0 (Ubuntu/Linaro 7.4.0-1ubuntu1~18.04.1)) #1 SMP PREEMPT RT Tue Jul 9 03:07:27 PDT 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: Texas Instruments Keystone 2 Edison EVM
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000081f800000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node dsp-common-memory@81f800000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 64 MiB at 0x00000000eb000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: Using PSCI v0.1 Function IDs from DT
[ 0.000000] percpu: Embedded 17 pages/cpu @ea90e000 s37356 r8192 d24084 u69632
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 190820
[ 0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 earlyprintk root=/dev/ram0 rw
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 10, 4718592 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 667412K/770048K available (8192K kernel code, 485K rwdata, 2844K rodata, 2048K init, 10196K bss, 28908K reserved, 73728K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xef800000 - 0xff800000 ( 256 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef000000 ( 752 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0a00000 (10208 kB)
[ 0.000000] .init : 0xc0e00000 - 0xc1000000 (2048 kB)
[ 0.000000] .data : 0xc1000000 - 0xc10797d0 ( 486 kB)
[ 0.000000] .bss : 0xc1084378 - 0xc1a79688 (10197 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] RCU debug extended QS entry/exit.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] kmemleak: Kernel memory leak detector disabled
[ 0.000000] arch_timer: cp15 timer(s) running at 233.33MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x6ba0ac50b7, max_idle_ns: 881590427583 ns
[ 0.000004] sched_clock: 56 bits at 233MHz, resolution 4ns, wraps every 4398046511102ns
[ 0.000009] Switching to timer-based delay loop, resolution 4ns
[ 0.000214] keystone timer clock @233333333 Hz
[ 0.000512] Console: colour dummy device 80x30
[ 0.269839] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.269841] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.269844] ... MAX_LOCK_DEPTH: 48
[ 0.269846] ... MAX_LOCKDEP_KEYS: 8191
[ 0.269847] ... CLASSHASH_SIZE: 4096
[ 0.269850] ... MAX_LOCKDEP_ENTRIES: 32768
[ 0.269851] ... MAX_LOCKDEP_CHAINS: 65536
[ 0.269853] ... CHAINHASH_SIZE: 32768
[ 0.269855] memory used by lock dependency info: 4639 kB
[ 0.269857] per task-struct memory footprint: 1536 bytes
[ 0.269891] kmemleak: Early log buffer exceeded (1066), please increase DEBUG_KMEMLEAK_EARLY_LOG_SIZE
[ 0.270836] Calibrating delay loop (skipped), value calculated using timer frequency.. 466.66 BogoMIPS (lpj=2333333)
[ 0.270843] pid_max: default: 32768 minimum: 301
[ 0.271173] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.271185] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.273100] CPU: Testing write buffer coherency: ok
[ 0.273149] CPU0: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulnerable
[ 0.273736] /cpus/cpu@0 missing clock-frequency property
[ 0.382750] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.421311] Setting up static identity map for 0xc0200000 - 0xc0200138
[ 0.441174] Hierarchical SRCU implementation.
[ 0.504437] EFI services will not be available.
[ 0.541427] smp: Bringing up secondary CPUs ...
[ 0.546090] smp: Brought up 1 node, 1 CPU
[ 0.550226] SMP: Total of 1 processors activated (466.66 BogoMIPS).
[ 0.556639] CPU: All CPU(s) started in SVC mode.
[ 0.563241] devtmpfs: initialized
[ 0.611020] random: get_random_u32 called from bucket_table_alloc+0x158/0x298 with crng_init=0
[ 0.621724] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.635099] DMA-API: preallocated 4096 debug entries
[ 0.640199] DMA-API: debugging enabled by kernel config
[ 0.646500] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.656578] futex hash table entries: 256 (order: 3, 32768 bytes)
[ 0.663133] ------------[ cut here ]------------
[ 0.667892] WARNING: CPU: 0 PID: 1 at mm/cma.c:111 cma_init_reserved_areas+0xb4/0x274
[ 0.675890] Modules linked in:
[ 0.679073] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.14.79-rt47-ga72bf1418c #1
[ 0.679075] Hardware name: Keystone
[ 0.679077] Backtrace:
[ 0.679088] [<c020c500>] (dump_backtrace) from [<c020c7e4>] (show_stack+0x18/0x1c)
[ 0.679093] r7:60000013 r6:c106ad44 r5:00000000 r4:c106ad44
[ 0.679105] [<c020c7cc>] (show_stack) from [<c09a90b0>] (dump_stack+0x80/0x94)
[ 0.679112] [<c09a9030>] (dump_stack) from [<c021fdd8>] (__warn+0xec/0x104)
[ 0.679116] r7:00000009 r6:c0bd2d5c r5:00000000 r4:00000000
[ 0.679122] [<c021fcec>] (__warn) from [<c021fea8>] (warn_slowpath_null+0x28/0x30)
[ 0.679126] r9:c106cc8f r8:00000000 r7:c1084380 r6:c159b618 r5:c159b618 r4:0081f800
[ 0.679133] [<c021fe80>] (warn_slowpath_null) from [<c0e166c0>] (cma_init_reserved_areas+0xb4/0x274)
[ 0.679140] [<c0e1660c>] (cma_init_reserved_areas) from [<c02018c8>] (do_one_initcall+0x4c/0x16c)
[ 0.679145] r10:c0e46858 r9:c1084380 r8:c0e4683c r7:c1084380 r6:c0e1660c r5:00000000
[ 0.679147] r4:ffffe000
[ 0.679153] [<c020187c>] (do_one_initcall) from [<c0e01040>] (kernel_init_freeable+0x268/0x300)
[ 0.679157] r8:c0e4683c r7:c1084380 r6:00000002 r5:c0e61030 r4:c0cc5a5c
[ 0.679163] [<c0e00dd8>] (kernel_init_freeable) from [<c09bcfe4>] (kernel_init+0x10/0x120)
[ 0.679168] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09bcfd4
[ 0.679170] r4:00000000
[ 0.679178] [<c09bcfd4>] (kernel_init) from [<c0208720>] (ret_from_fork+0x14/0x34)
[ 0.679181] r5:c09bcfd4 r4:00000000
[ 0.679183] ---[ end trace 0000000000000001 ]---
[ 0.822456] Unable to handle kernel paging request at virtual address fb2aa000
[ 0.829833] pgd = c0003000
[ 0.832654] [fb2aa000] *pgd=800000c0007003, *pmd=00000000
[ 0.838208] Internal error: Oops: 206 [#1] PREEMPT SMP ARM
[ 0.838211] Modules linked in:
[ 0.838217] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.14.79-rt47-ga72bf1418c #1
[ 0.838220] Hardware name: Keystone
[ 0.838223] task: ea058000 task.stack: ea054000
[ 0.838229] PC is at cma_init_reserved_areas+0xf8/0x274
[ 0.838232] LR is at __warn+0xb4/0x104
[ 0.838236] pc : [<c0e16704>] lr : [<c021fda0>] psr: 60000013
[ 0.838239] sp : ea055e90 ip : ea93c000 fp : ea055edc
[ 0.838241] r10: 00000000 r9 : c106cc8f r8 : 00000000
[ 0.838244] r7 : c0bd2d5c r6 : c159b618 r5 : 0081f800 r4 : 0081f800
[ 0.838247] r3 : 1096e000 r2 : 000003c0 r1 : 00000024 r0 : 0075f800
[ 0.838252] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 0.838255] Control: 30c5387d Table: c0003000 DAC: fffffffd
[ 0.838258] Process swapper/0 (pid: 1, stack limit = 0xea054210)
[ 0.838261] Stack: (0xea055e90 to 0xea056000)
[ 0.838265] 5e80: c02ef684 c159b618 c159b618 014080c0
[ 0.838270] 5ea0: c1012ac4 c1598d80 00000000 00000002 c1084380 ffffe000 00000000 c0e1660c
[ 0.838275] 5ec0: c1084380 c0e4683c c1084380 c0e46858 ea055f4c ea055ee0 c02018c8 c0e16618
[ 0.838279] 5ee0: ea055f04 ea055ef0 c027af00 c0bbff98 c0bbff78 c0bbffc4 c0bd31b8 00000000
[ 0.838283] 5f00: c0bbff0c c0c676e4 00000001 00000001 c106d368 c0cc5a5c eafffdfd 00000000
[ 0.838287] 5f20: c10191b0 c0cc5a5c 00000002 c0cc5a5c c0e61030 00000002 c1084380 c0e4683c
[ 0.838291] 5f40: ea055f94 ea055f50 c0e01040 c0201888 00000001 00000001 00000000 c0e00644
[ 0.838295] 5f60: c0e00644 000000e8 00000000 00000000 c09bcfd4 00000000 00000000 00000000
[ 0.838298] 5f80: 00000000 00000000 ea055fac ea055f98 c09bcfe4 c0e00de4 00000000 c09bcfd4
[ 0.838302] 5fa0: 00000000 ea055fb0 c0208720 c09bcfe0 00000000 00000000 00000000 00000000
[ 0.838306] 5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.838310] 5fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 0.838312] Backtrace:
[ 0.838320] [<c0e1660c>] (cma_init_reserved_areas) from [<c02018c8>] (do_one_initcall+0x4c/0x16c)
[ 0.838326] r10:c0e46858 r9:c1084380 r8:c0e4683c r7:c1084380 r6:c0e1660c r5:00000000
[ 0.838328] r4:ffffe000
[ 0.838333] [<c020187c>] (do_one_initcall) from [<c0e01040>] (kernel_init_freeable+0x268/0x300)
[ 0.838338] r8:c0e4683c r7:c1084380 r6:00000002 r5:c0e61030 r4:c0cc5a5c
[ 0.838342] [<c0e00dd8>] (kernel_init_freeable) from [<c09bcfe4>] (kernel_init+0x10/0x120)
[ 0.838347] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09bcfd4
[ 0.838349] r4:00000000
[ 0.838355] [<c09bcfd4>] (kernel_init) from [<c0208720>] (ret_from_fork+0x14/0x34)
[ 0.838358] r5:c09bcfd4 r4:00000000
[ 0.838363] Code: e34c70bd e50b5044 e1a05004 e50b6048 (e79c3003)
[ 1.102100] ---[ end trace 0000000000000002 ]---
[ 1.106848] Kernel panic - not syncing: Fatal exception
[ 1.112215] ---[ end Kernel panic - not syncing: Fatal exception
[ 2.343849] workqueue: round-robin CPU selection forced, expect performance impact
I cant boot kernel with a specific memory range(0xD0000000-0xF8000000), not boot with bigger range (0x80000000-0xFFFFFFFF) too with different reason.
I tried a lot of ways and research from a lot of websites, but cant find a solution. Same error for both configuration is "Unable to handle kernel paging request at virtual address ********, pgd = 0xD0003000". I noticed that the 0xD0003000 address is the first function RAM address in 'System.map'. Is it possible to kernel can not reach RAM addresses? Can i use directly phsical mapping instead of virtual mapping?
00000024 A cpu_ca15_suspend_size
00000024 A cpu_v7_bpiall_suspend_size
00000024 A cpu_v7_suspend_size
0000002c A cpu_ca9mp_suspend_size
d0003000 A swapper_pg_dir
d0008000 T _text
d0008000 T stext
How can i boot kernel with specific memory ranges and independently from uboot? By the way, i run linux with below steps on CCSv6;
Connecting ARM Core 0,
Load zImage to DDR(specified memory range start addr(if conf1: 0xD0000000, if conf2: 0x80000000),
Load keystone-k2e-evm.dtb to DDR (specified memory range area (if conf1: 0xF0000000, if conf2: 0x87000000)),
PC: zImage Load Addr,
R0: 0x00000000,
R1: 0xFFFFFFFF,
R2: keystone-k2e-evm.dtb Load Addr,
Run ARM Core 0
Thank you,
Best Regards,
Srt