This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3356: External Memory Compatibility Check

Part Number: AM3356

Tool/software: Linux

We're selecting external NAND and DDR3/L for an AM3356 project and we want to check if any of the below devices have been confirmed to work with the AM335x and any version of Linux.

  • SkyHigh SLC NAND S34MS08G2 or S34MS16G2
  • Micron DDR3L MT41K512M16
  • NANYA DDR3L NT5CB256M16ER
  • Windbond DDR3 W634GG6MB

I have a pretty high confidence on the DDR3 devices based on the datasheets, except for the Micron MT41K512M16 which is a "twin die" device. This E2E post suggests that "dual die" DDR3 are not compatible with AM335x but recommends the MT41K512M16 which is a dual die device.   

Thanks in advance,

Ruben