Hello,
I'm researching a potential AEW/AWB solution on the DM6446 mated with a CMOS Bayer sensor, and i wanted to get some bits of information about the existing 3A hardware:
1) Although there exists a AEW and AWB driver for the DM6446 (LSP 1.20), can a designer completely develop a full control loop solution based on existing public domain documentation on this? These docs in question would be the VPFE datasheet, as well as the PSP driver documents for both of these drivers.
2) Is there existing IP available from TI?
Thank you.