Part Number: AM4378
Hello
I am using AM4378 to create a UART receiver circuit.
data: 8bit
bps: 230400
parity: none
stopbit: 1 bit
In rare cases, sending a 1000-character packet may result in the loss of one or more characters.
Technical Reference Manual -Table 21-6. UART Mode Baud and Error Rates
There is "Error Rates" in the above specification, and there is a 0.16% Error at 230400 bps. Is this the cause?
Is there any way to avoid it?
Thank you in advance.