could you please provide Linux driver source code which supports both HSR and PRP.
This driver has mentioned in section 4.2.3.3.1 in below link
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
could you please provide Linux driver source code which supports both HSR and PRP.
This driver has mentioned in section 4.2.3.3.1 in below link
Hi,
Which device is this?
In general this is part of the prueth, located in drivers/net/ethernet/ti in Processor SDK Linux. There is also the /net/hsr-prp which contains some protocol specific resources.
You can download Processor SDK Linux for AM572x from here:
Best Regards,
Yordan