This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6747: USB1 Unused pin handing

Part Number: TMS320C6747

Hello,

My customer is needed to move over from the current DA810 to C6747 without hardware design change. They would like to confirm unused pin handing for USB1_DP and USB1_DM. C6747 datasheet mentions those pins should be leaved unconnected. But in the current DA810 based HW design, those have been connected to GND (Because those pins are regarded as GND pins in DA810 datasheet). 

Do you have any concerns for leaving those pins connected to GND ?

Best Regard,
NK