Part Number: 66AK2H06
Hi
I have following queries..
1) How many MACs are there in 66AK2H06 ?
2) Are all are configurable ?
3) Is it possible for any device (connected at port 1) to exchange data with any other device (connected at port 2 / 3 / 4) without passing it through processor (i.e at port 0) ?
4) if it is possible (point 3 above), can we restrict it with the use of MAC IDs ?
Regards