Tool/software: Code Composer Studio
Hello,
I am using TMS320C6748 with dsplib_c64Px_3_4_0_0 (I purposely using the fixed point DSP lib as my Input will be fixed point so I am purposely avoiding to use dsplib_c674x_3_4_0_0). Now i have strange issue which i guess somebody have already seen. As i have lots of Complex computation and using _cmpyr and _cmpyr1 intrinsic so as per it my Real Samples are at MSB and Imag samples at LSB place (based on Sprugh7 section 4.60.
As i am using DSP_fft16x16 it says "The arrays for the complex input data x[], complex output data y[] and twiddle factor w[] must be double word aligned. The input and output data are complex, with the real/imaginary components stored in adjacent locations in the array. The real components are stored at even array indices, and the imaginary components are stored at odd array indices."
Now if i have to use _cmpyr real should be odd place but DSP_fft16x16 wants it to be in even place. I can do _rotl on the input data but that's not optimized approach. Can someone please tell me what i should do.
Also my project configuration is for _LITTLE_ENDIAN