Part Number: AM5718
Tool/software: Linux
Hi everyone,
On our custom am5718 board, we have HDMI connected as attached image. If we remove the ADV7611 and ADV7393 from our HDMI path, we are able to run ksmcube application and is running without issue. But with the above chips included, we are not seeing anything on the diplay. Using modetest command, it is listing the diplay details. we have added adv7393 and ADV7604(for supporting ADV7611) in our menuconfig and both are detected properly in linux as verified from the Linux boot prints. Someone pls help us with this issue? Should i modify anything on the default configuratuion in drivers given or same default configuration will work?
Linux Version : linux-4.14.67+gitAUTOINC+d315a9bb00-gd315a9bb00
Regards,
Noufal P