This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: Running Linux TIDL exmaples on VAYU VISION APPLICATION BOARD

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: AM5749, AM5746, AM5706, AM5708

Tool/software: Linux

Hello,

We have an "ASSY 516620 - VAYU VISION APPLICATION BOARD".

Our goal is to build a Linux image that has tidl examples.

In order to build the Linux system - we used the instructions as described in VisionSDK_Linux_DevelopmentGuide.pdf.

The VisionSDK version is 03_06_00_00.

No problems with the Linux image that we built and is up and running.

But, we want to run the tidl examples described here: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_TIDL.html

The link above is related to Processor SDK 06_00_00_07, and it seems that our board is not in the support list:

  • AM5749 (2xEVEs + 2xC66x DSPs)
  • AM5746 (2xC66x DSPs)
  • AM572x (2xC66x DSPs)
  • AM571x (1xC66x DSP)
  • AM5706 (1xC66x DSP)
  • AM5708 (1xC66x DSP)

The examples we want to run are:

  • Imagenet classification
  • Segmentation
  • SSD_Multibox
  • Classifications with Class filterning
  • Unit Tests

But, they are not part of the image that we created using VisionSDK version is 03_06_00_00.

Instead, vision_sdk_load.sh and apps.out were provided - but no tidl.

Question:

  1. Should we use the TI SDK instead of VisionSDK, and repeat the whole buildup process, though the device is not listed? In that case  - we need to know which flags and environment variables should be used
  2. If not, what should we do in order to import and build theses examples, or the their equivalent on our EVM

Thank you