This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: DDR3 bit width questions

Part Number: AM5728

Tool/software: Linux

Hi,TI

check the TI data sheet and see that two EMIF buses are available in the AM5728 chip, EMIF1 and EMIF2, respectively.

Currently TI's design, both EMIF1 and EMIF2 are mounted with two 16bit DDR3 chips. Then the bus bit width of EMIF1 and EMIF2 should be 32-bit.

So when testing with tools such as stream, should the bit width of the EMIF bus be 32-bit, or 64-bit?

DDR3 theoretical rate = 1066MT/s * 32 bit = 4.2GB/s or DDR3 theoretical rate = 1066MT/s * 64 bit = 8.5GB/s.

which one is correct ?

please let me know that,

Thanks.