Other Parts Discussed in Thread: AM5728, TPD12S015, TPD12S016
Tool/software: Linux
Hai all,
We have one custom board where AM5718 is used. We are facing some strange errors if we connect different monitors to the board.
I have tested the same observation with EVM and it is working without any problem.
Scenario-1:
EVM and Custom boards connected to monitor (Dell U2413F) . I have run both modetest and kmscube, working fine.
Scenario-2:
EVM connected to monitor (SAMSUNG LA40M81BM-It is a TV which supports HDMI connection). And works fine without any problem.
Scenario-3:
Custom board connected to monitor (SAMSUNG LA40M81BM-It is a TV which supports HDMI connection).
1) If i connect the monitor after logging in, then started observing some prints on uart console like below line.
omap_i2c 48070000.i2c: controller timed out
omap_i2c 48070000.i2c: controller timed out
omap_i2c 48070000.i2c: controller timed out
cpu cpu0: vdd failed for 1060000uV[min 850000uV max 1500000uV]
cpufreq: __target_index: Failed to change cpu frequency: -110
omap_i2c 48070000.i2c: controller timed out
omap_i2c 48070000.i2c: controller timed out
omap_i2c 48070000.i2c: controller timed out
2) if monitor is connected during boot time and the after
omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
[ 3.586406] hctosys: unable to open rtc device (rtc0)
[ 3.592124] ALSA device list:"
prints, booting is very slow and also it shows prints like below,
omap_i2c 48070000.i2c: controller timed out
omap_i2c 48070000.i2c: controller timed out
cpu cpu0: vdd failed for 1060000uV[min 850000uV max 1500000uV]
Can anyone please help regarding this issue??
Linux used: 4.14.67
SDK: 05.01.00.11
Regards,
Noufal P