This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA750: SD Card High speed Mode CLK frequency

Part Number: DRA750

As per SD card standard the CLK frequency in high speed should be 50MHz, but in the DRA75x datasheet it is mentioned as 48MHz? could you please confirm it is correct value?

Because I'm using an SD card interface at MMC1, the SD card datasheet says its supporting clock frequency as 50MHz in high speed mode. So per standard the host should support 50MHz right?

Thanks

Manoj.