This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISS module is not going to disable.

Hi,

To disable ISS module writing PM_ISS_PWRSTCTRL (0x4AE0 7C80) register bits 1:0 to "00", So its power state will be in off state. But for testing purpose reading the PM_ISS_PWRSTST(0x4AE0 7C84) register which showing ISS in ON state. How to change the status of ISS power status register to off state?

To disable EVE module sequence followed is:
1.Change module state to off state

2. Reset the EVE module.

3. Change the clock state to hardware dependent. 

This sequence will disable the clock state as well as power state.

Is it correct sequence for to disable EVE?|

There is no reset functionality for ISS module.

Thank You!

Sagar