Other Parts Discussed in Thread: AM3354
Tool/software: Linux
I have a custom board of which cpu is AM3354.It doesn't have EEPROM and RTC. I disabled the RTC and EEPROM detected related module during u-boot and now u-boot is able to boot. But the kernel is hanging after print "Uncompressing Linux... done, booting the kernel." After a while, the cpu automatically reset.
I used the printascii and located the error happened in __turn_mmu_on:
mcr p15, 0, r0, c1, c0, 0 @ write control reg
mrc p15, 0, r3, c0, c0, 0 @ read id reg
instr_sync
What should I do to solve the problem?
In addition, if I don't have an RTC chip, should RTC_PWRONRSTn be pulled low?
I would be grateful if I could get a reply as soon as possible.Thank you!