This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: Boot ROM error check

Part Number: AM3358

Hi,

I was wondering for the AM3358 what takes care of the error checking for boot rom?

Is it the on chip memory controller?

For Instance a system on the boot ROM to prevent single bit flip from resulting in an unbootable system?

In this case could fall under a parity check, however in technical reference manual section 7.2 OCMC-RAM

It states Parity is not supported under unsupported features, is there any other part of the processor that takes care of this?