This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355 SD Card Remounting after Ejecting

I'm seeing a problem with ejecting an SD card on the DVEVM after it has been mounted, in that when the card is reinserted it is no longer accessible (in fact trying to reaccess it gives a whole load of errors). After a bit of digging I found in the directory on the PC installation........

/dvsdk_1_30_00_40/PSP_01_20_00_014/lsp_psp_01_20_00_014_release_notes.html

....which says "DM355/DM6446: Removing MMC/SD card when mounted leads to unusable access and can not umount.    Workaround: Unmount MMC/SD card before removing it.

I have tried as suggested unmounting before removal (ie. simply using umount), and then remounting when reinserted, and it works fine. Though for the production application it would need 'hot' removal and reinsertion.

Could you tell me please if an update is available that fixes this, or if it has a planned fix.

Many thanks