This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4376: DMA FIFO size

Part Number: AM4376

Tool/software: Linux

Hi all,

I have a quite slow GPMC device: 190 ns per byte.

So, the idea was to use DMA for async access.

I've started DMA read access over 16 KByte and tried to get with memcpy 2 bytes simultaneously.

Measured time for these 2 bytes was 97 usec. That results from 512 bytes X 190 ns DMA access.

Question: Is there a possibility to configure FIFO size ? I would prefer to work with 32 bytes instead of 512.