Tool/software: Linux
Hi,
I got this hardware below.
a. TDA2Px EVM x 1
b. Fusion Card/EVM x 1
c. TIDA OV2775 cameras (with Fakra cables) x 1
I can capture the image from OV2775_TIDA1130 in Linux in vision_sdk with ISS Usecases, (TDA2Px ONLY)/1CH ISS Capture + ISP + DISPLAY. Now I want to port my customer camera.Before that, I want to learn the framework. And I think this usecase is good to use.
At first I thought the driver sources is in vision_sdk/apps/src/rtos/iss/src/sensor/ov2775 .But it seems I was wrong, I modified the code, and rebuild and copied the app.out to evm and ran it.It didn't work as I wanted.
I compared the md5 of app.out before modify and after. It hasn't changed.
So,Which source files do OV2775_TIDA1130 use?
Thanks and Regards
CalmCar