Other Parts Discussed in Thread: MMWCAS-DSP-EVM, TDA2
Hello
I have as MMWCAS-DSP-EVM and want to use this to run RADAR Use case under the PROCESSOR_SDK_RADAR_03_07_00_00.
I have compiled the PROCESSOR_SDK_RADAR_03_07_00_00 with use case for tda2xx_cascade_bios_radar and then followed following the steps mentioned in VisionSDK_UserGuide_TDA2xx.pdf
1) section 3.6 (Load using SD card )
2) 3.6.1 (Option 1: Steps to prepare a bootable SD card )
3) 3.6.3 (Steps to generate MLO)
4) 3.6.4 (Steps to generate appImage)
5) 3.6.5 (SD Card setup)
Now when i try to plug the SD card into the MMWCAS-DSP-EVM board doesn't boot up.
If anybody can tell me what is the issue it will be really helpful for me.
Br
Deepak Joshi