I want to connect DM355 with a FPGA using the generic YCbCr interface of VPFE.
My video is 1280*960,4:2:2 format,line-by-line scanning.
So ,I want to use the generic YCbCr interface ,16bit wide ,the pclk will be 54M with the vpssclk 108M.
I see the datasheet of "TMS320DM335 Digital Media System-on-Chip Video Processing Front End.pdf".
But,I don't know the time sequence of Y[0..7],C[0..7],and HD,VD,PCLK.
There is not anything about the time sequence in that datasheet.
How can I put the YCbCr data into DM355 with this interface?