Hey,
I am using PSDK3.5 with TDA2PXEVM. I want to change the MMC instance from 1(which is currently used) to 3, to test if file writing with 8bit data bus will accelerate writing frames to sd card.
So far I can`t find where to change the MMC and if it is possible at all.
Where can I adjust the settings to use MMC3?
Also I would like to increase the clk frequency from 10MHz to 19MHz in order to speed up the writing process. Does this work?
regards,
Nicolas Rausch