This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLACKHAWK USB560BP

I bought a BLACKHAWK USB560BP. I can use it to connect my DM6467 and DM6446 Platform with the config file supplied by blackhawk setup software. But I can't connect to the DM355 platform. It always says

" Trouble Reading Memory Block at 0x1c40900 on Page 0 of Length 0x4:
Error 0xC0002044/-181
Error during: Register, Initialization, Control,
This error was generated by TI's USCIF driver.

SC_ERR_CTL_NO_TRG_CLOCK <-181>
The controller has detected a dead JTAG clock.
The user must turn-on or connect the JTAG clock for the target.
"

But I can use my PCI XDS560 to connect the DM355 platform. What's the problem about the BLACKHAWK USB560BP? Is the config file supplied by blackhawk is wrong?

  • I solve it now. The problem is due to the switcher.

    When I use the PCI emulator, I set the switcher to NAND boot. I can connect the emulator to DM355 on this mode.

    But when I use USB emulator, I can't connect the emulator to DM355 on this mode. I have to set the switcher to other boot mode.