Other Parts Discussed in Thread: TMS320DM355
HI everyone.
I just started using the DM355EVM pcb with the software supplied on the CD's, setup the
development environment, tool chain etc, compiled the kernel using the defaults, .
and setup the target root file system via NFS. I flashed in the uImage via uBoot and can boot up
the 2.6.10-mvl401 kernel using the NFS root.
I cabled the TV out into a DVR and connected the DVR VGA output to a display. I can
run the dvevmdemo and see the video output on my VGA display.
I'm having a problem running X. When I startx, I see some console display initially which
must have been in the frame buffer, so it sort of works. I set the DISPLAY env var to davincifb.vido
When I try to run any X app, ie xlogo, I get a "Can't open display: davincifb.vid0" error.
I've been checking the forum and google, but haven't come up with much so far. Can anyone
point me to any info on how to set this up ?
Thanks,
John