Tool/software: TI C/C++ Compiler
Hi, I'm compiling ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01 times the following error:
It seems to be unable to access the website, how to solve?
**********************************************
Do you want to fetch all the sources y/N
[ n ]y
error: command 'sync' requires repo to be installed first.
Use "repo init" to install it here.
error: command 'forall' requires repo to be installed first.
Use "repo init" to install it here.
Do you want to extract linux-devkit y/N
[ n ]y
conjunction@publish:~/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01$ repo init
fatal: Cannot get gerrit.googlesource.com/.../clone.bundle
fatal: error [Errno 101] Network is unreachable
fatal: cloning the git-repo repository failed, will remove '.repo/repo'