This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5504 GPIO[18:20,27] instead of I2S2

Other Parts Discussed in Thread: TMS320C5504

Sorry for the innane post, but I have been through sprugh6 (TMS320C5504 DSP System User's Guide), sprufo4 (General-Purpose Input/Output) and sprufx4 (Inter-IC Sound (I2S) Bus) a few times and seem to be missing something obvious.

I know that the PPMODE bits in the EBSR are responsible for the pertinent pin multiplexing (per sprugh6 section 1.7.3.1 External Bus Selection Register).  Only two of those modes apply to a device without the LCD controller; 001 and 110.  I currently am setting the PPMODE bits to 001 because this is indeed the peripheral set that I need sans the I2S2.  In other parts of the EBSR definition I see bitfields for reconfiguring I2S0 (SP0MODE) and I2S1 (SP1MODE) as GPIO, however I cannot seem to find any such setting for I2S2.  Am I just blind, or did I make a mistake in assuming that I could reconfigure these pins as GPIO?

Thanks in advance,

Gary