This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Debug GEL file

Part Number: TMS320C6748

Hi,

Does the Debug GEL file mentioned in the link  http://www.ti.com/lit/an/spracm8/spracm8.pdf  still available? There are no diagnostics info like:

• ROM ID: Revision number of the boot ROM • Silicon revision number

• Boot Mode: Current boot mode, as selected by the boot pins latched at reset

• ROM Status Code: Current status of the ROM code

• Description: Description of any error messages that the ROM may have encountered during boot

• Program Counter: The current program counter of the connected device ( or DSP)

• Device Information: Generic device information that may be helpful when getting support from TI

• Clock information: PLLm_SYSCLKn is output

in CCS_INSTALL_PATH\ccs_base\emulation\boards\evmc6748\gel.