Hi everybody ,
I m in Android 4.3 and using a WIFI module attached via SDIO signals .
WIFI module can work @ 3.3 V or 1.8V SDIO IO signals , and I am on eMMC1 .
now using signals @ 3.3V everything is fine . if I use 1.8V level ( with proper settings etc ) module is not working .
what I noticed using a scope --> no signal or bus activity by DRA744 at all , all signals are stuck if IO are set @ 1.8V
I noticed in TRM you need to start @ 3.3 V on IO on SDcard ( it is in table 25-2 ) : is this needed also for SDIO ? ( in the TRM it seems not ..)
please where am I wrong ?
best regards
Carlo