This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA722: I2C pull-up register value

Part Number: DRA722

Hello,

Now using 10kohm PU register on I2C lines, based on VOL and Idrive specification in data manual and EVM's I2C pull-up register value.

However, the actual measurement on the board, tr timing value was 600nsec and not meet the fast speed tr specification (max 300ns).

Is there any recommended PU register value of I2C (fast speed)?

Regards,

Takeo

  • Takeo-san,

    The required resistor value will depend on the PCB capacitance.  You should experiment to reduce the resistor value to find the appropriate rise time.  It sounds like 5k may work for your needs.

    Thanks,

    Kyle