Part Number: AM5728
Hi,
I am using the AM5728 PROCESSOR in our board.All the PMIC(TPS6590378) outputs are coming correctly within tolerance and also checked for the clk in for OSC0,1.
Both the clocks are OK. Then i connected UART3-RS232 converter output to the PC.I have done the basic setting for the serial port Baud--> 115200,data size--> 8,parity--> none etc.
There is no reply/reponse from the processor.
Is any other thing i need to check?
Is UART3 respond from the ROM boot loader or some boot image file require?
Please provide the feedback and related link .
Thanks in advance.