Part Number: AM3715
Hello,
customer has problem to receive on UART2 under Linux. No RX interrupt. There are nothing in the receive register. Transmission is ok.
UART1 works w/o problem. UART3 o, but has problems with the debug output which hangs.
The UARTs 1...3 uses the same driver „TI, omap3-uart“. The problem with the UART2 is seen with Linux and also with WinCE.
Is there any receive problem with the UART2?
Regards, Holger