This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: The program when use both CS0 and CS1

Part Number: TMS320C6678

Tool/software: Code Composer Studio

There are 10 ddr chips. Five chips is on the front of the board and connected to CS0, anthor five chips is on the back of the board and connected to CS1. There are one chip for ecc in every five chips.

The data width of each ddr chip is 16 bits .

There are no problems when the ddr frequency is below 1000MHz, also include 1000MHz. But the problem in picture below is arised when the frequency is 1600MHz. The picture below was got from high-speed oscilloscope.

My question: how to adjust the phase of clock to meet timing requirement.