Part Number: TDA2P-ACD
Tool/software: Linux
Hi,
How can I raise DSP frequency to 1GHz?
Currently, when I run "omapconf show opp" this is the output.
| VDD_DSPEVE / VDD_CORE3 | 33C / 91F | NA | | PLUS |
| DSP1 | | | 850 MHz | |
| DSP2 | | | 850 MHz | |
| EVE1 | | | 900 MHz | |
| EVE2 | | | 900 MHz | |
In TRM it says that OPP_PLUS is supported and max frequency is 1GHz for DSP, but I have 850MHz.
Thanks in advance,
Igor