This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535: USB Mass Storage Device implementation with SPI NOR Flash

Part Number: TMS320C5535

Hi,

I have a SPI NOR Flash device with TMS320C5535 and would like to transfer file from PC to the Flash via USB.

Is there any example code that I can refer to as device needs to have a file system. 

I saw the USB Full Speed Example Project in the Chip Support Library 3.08 but that uses transfer of files between PC and MMC/SD Card.

As mine is a 'raw' device how do I go about it.

Thanks and Regards,

Sangeeta Gunwani