Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hi all,
I created the NIMU_BasicExample_evmAM437x_armExampleproject for my AM437x EVM via the pdkProjectCreate.bat file:
pdkProjectCreate.bat AM437x evmAM437x little nimu all arm
However when importing the created project into a workspace and building it, I receive the following warning:
"_SYS_SELECT_H" redefined
According to the build log the first definition can be found at c:\ti\bios_6_75_02_00\packages\gnu\targets\arm\libs\install-native\arm-none-eabi\include\sys\select.h, whereas the warning (redefinition) occurs in the socketndk.h file
Why is this warning present in a generated example project? Is it a known warning that I should be concerned about or can it be ignored?
The following is true for my setup:
- CCS Version: 9.1.0.00010
- Processor SDK: v1_0_14
- ndk_3_40_01_01
- GNU v7.2.1 (linaro)
Regards,
Johhny