This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDKTCPIP: NDK_accept() fails with EINVAL accidentally

Part Number: NDKTCPIP

Hi there,

I run into an issue NDK_accept() returning EINVAL accidentally despite it shouldn't.

I think I found a bug in NDK implementation. I debugged it in v2.25.0.9, the code of current c2.25.1.11 looks the same (stack/fdt/socket.c):

SOCKET NDK_accept( SOCKET s, PSA pName, int *plen )
{
    FILEDESC *pfd = (FILEDESC *)s;
...
    /* If there's a name, there must be a valid length */
    if (pName && (!plen || (pName->sa_family == AF_INET && *plen < sizeof(SA_IN)) 
#ifdef _INCLUDE_IPv6_CODE      
        || (pName->sa_family == AF_INET6 && *plen < sizeof(SA_IN6))
#endif
       ))
    {
        error = EINVAL;
        goto accept_error;
    }
...
    /* Get the connected address */
#ifdef _INCLUDE_IPv6_CODE      
    if (pfd->Type == HTYPE_SOCK6)
    {
        if (pName)
            Sock6GetName(pfdnew, 0, pName);
        if (plen)
            *plen = sizeof(SA_IN6);
    }
    else
#endif
    {
        if (pName)
            SockGetName(pfdnew, 0, pName);
        if (plen)
            *plen = sizeof(SA_IN);
    }
...
}

The code checks pName->sa_family to decide if it expects IPv4 or IPv6 and thus checks if the size of the struct is sufficient for IPv4 or IPv6 either.

The documentation (spru524j) clearly says "The argument addr is a result parameter that is filled in with the address of the connecting entity as known to the communications layer." So the code should not check its contents! As I called NDK_accept() with pName as a reference to an uninitialized local var NDK_accept() checked some value in the stack. Depending on the program flow history pName->sa_family happened to be AF_INET6 (10). As I am working with IPv4 it complained about the size of the struct being less than sizeof(SA_IN6) and returned unexpectedly with EINVAL.

Since NDK_accept() decides depending on pfd->Type == HTYPE_SOCK6 if it wants to fill a SA_IN6 or SA_IN struct I think it should check pfd->Type too to decide which size it expects.

I changed

    if (pName && (!plen || (pName->sa_family == AF_INET && *plen < sizeof(SA_IN)) 
#ifdef _INCLUDE_IPv6_CODE      
        || (pName->sa_family == AF_INET6 && *plen < sizeof(SA_IN6))
#endif
       ))

to

    if (pName && (!plen || ((pfd->Type == HTYPE_SOCK) && *plen < sizeof(SA_IN))
#ifdef _INCLUDE_IPv6_CODE
        || ((pfd->Type == HTYPE_SOCK6) && *plen < sizeof(SA_IN6))
#endif
        ))
and now it works fine for me.

May be you want to accept this bugfix ...

Best regards,
Lars

  • Hi Lars,

    Which device is this? Which Processor SDK RTOS?

    Best Regards,
    Yordan

  • Dear Lars,

    be aware that "spru524j" is not the latest version of that document.
    Please use this link to download the actual version -> www.ti.com/lit/spru524

    Regards, Bernd

  • Hi Yordan,

    I'm using a DM8147 with SYS/BIOS v6.35.6.56. But this actually doesn't matter, the issue is inside the NDK stack. As far as I've seen v2.25.1.11 seems to be the most recent version.

    Best regards,
    Lars

  • Hi Bernd,

    I referenced "spru524j" as it came with the NDK v2.25.1.11. I just checked "spru524k" - regarding the addr/pName parameter of accpet()/NDK_accept() it reads exactly the same.

    Best regards,
    Lars

  • Lars,

    DM814x device comes with EZSDK 5.05.02.00.

    This EZSDK package has bios_6_33_05_46 package, but there is no NDK package inside the EZSDK. From what I understand you have downloaded bios_6_35_06_56 and ndk_2_25_01_11 packages, and trying to port these into DM814x EZSDK software, is that correct?

    Note that ndk_2_25_01_11 package requires bios_6_45_00_20 and also below components versions:

    Note also that the latest NDK package version is 3.60.00.13 and comes with AM335x RTOS package:

    software-dl.ti.com/.../index_FDS.html

    Regards,
    Pavel

  • Hi Pavel,

    yes, we started DM814x development several years ago based on our previous DM643x project. I think we started with NDK v2.22.03.20 at that time and updated to NDK 2.25.00.00 later. I remember we had some issues with newer SYS/BIOS versions, so we kept v6.35.6.56. This combination works fine for years now and we still continue to provide updates to our customers based on that platform.

    From looking at the code I'm very sure the issue I described has nothing to do with the SYS/BIOS version or processor model actually used. Once again in short: The NDK code evaluates data in a result only argument - that's simply not correct!

    I wonder if the issue is still part of the current NDK release. (Just to help others running into the same problem.) Is there a separate NDK 3.60.00.13 download available? I'm not keen on downloading and installing a 700MB SDK for a processor family we don't use just to check one line of code.

    May be you could check the code of the accept() function of NDK 3.60.00.13 if the code changed. (Or provide this code to me directly so I could have a look.)

    Best regards,
    Lars

  • Lars,

    The latest user guide regarding NDK_accept() is SPRU524K:

    The latest NDK files regarding NDK_accept() are:

    ndk_3_60_00_13/packages/ti/ndk/inc/socket.h
    ndk_3_60_00_13/packages/ti/ndk/inc/socketndk.h
    ndk_3_60_00_13/packages/ti/ndk/stack/fdt/socket.c
    ndk_3_60_00_13/packages/ti/ndk/slnetif/slnetifndk.c

    I am attaching these files:

    6013.socket.h

    8814.socketndk.h

    /*
     * Copyright (c) 2012-2019, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * */
    /*
     * ======== socket.c ========
     *
     * This file handles core BSD style socket calls and pipes.
     *
     */
    #include <stkmain.h>
    #include "fdt.h"
    
    /* NDK_HookFxn funtion pointers */
    NDK_HookFxn NDK_createSockCtx = NULL;
    NDK_HookFxn NDK_closeSockCtx = NULL;
    NDK_HookFxn NDK_netStartError = NULL;
    
    /**********************************************************************
     ************************* Socket Handling Functions ******************
     **********************************************************************/
    
    /**
     *  @b Description
     *  @n
     *      This function extracts the first pending connection request
     *      in the socket queue and spawns a new socket to accept the
     *      incoming connection request. This function call is valid only
     *      for connection-oriented socket types like TCP.
     *
     *  @param[in]  s
     *      Handle to local bound socket that is waiting/listening on
     *      any incoming connections. The argument s is a socket that
     *      has been created using "socket" function call, bound to a
     *      local address using "bind" and listening for connections
     *      with "listen" function calls.
     *
     *  @param[in]  pName
     *     Handle to the sockaddr structure that holds the peer host's
     *     address and port information.
     *
     *  @param[in]  plen
     *     Holds the length of the sockaddr structure being passed as
     *     argument to this function.
     *
     *  @param[out]  pName
     *     Handle to the sockaddr structure that holds the connected peer's
     *     address and port information. The exact format of this is
     *     based on the address family. Valid only when this function returns
     *     success.
     *
     *  @param[out]  plen
     *     Holds the length of the connected peer's sockaddr structure.
     *     The exact length depends on the address family of the socket
     *     created. Valid only when the function returns success.
     *
     *  @retval
     *      Success -   Handle to the new socket created
     *  @retval
     *      Error   -   INVALID_SOCKET
     *
     */
    SOCKET NDK_accept( SOCKET s, struct sockaddr *pName, int *plen )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        FILEDESC *pfdnew;
        int      error = 0;
    
        llEnter();
    
        /* Validate Input */
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return INVALID_SOCKET;
        }
    
        /* If there's a name, there must be a valid length */
        /*
         * Note64: sizeof returns size_t, which is 64 bit unsigned for
         * LP64. May need to cast to int32_t to avoid implicit type conversions
         */
        if (pName && (!plen || ((pName->sa_family == AF_INET) &&
            (*plen < (int)sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
            || ((pName->sa_family == AF_INET6) &&
            (*plen < (int)sizeof(struct sockaddr_in6)))
    #endif
           ))
        {
            error = NDK_EINVAL;
            goto accept_error;
        }
    
        /* Accept the new socket */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if (error = Sock6Accept(pfd, (void **)&pfdnew))
                goto accept_error;
        }
        else
    #endif
        {
            if (error = SockAccept(pfd, (void **)&pfdnew))
                goto accept_error;
        }
    
        /* Get the connected address */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if (pName)
                Sock6GetName(pfdnew, 0, pName);
            if (plen)
                *plen = sizeof(struct sockaddr_in6);
        }
        else
    #endif
        {
            if (pName)
                SockGetName(pfdnew, 0, pName);
            if (plen)
                *plen = sizeof(struct sockaddr_in);
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd(pfd, 0);
    
        llExit();
    
        /* Return the file descriptor table index */
        return (pfdnew);
    
    accept_error:
        /* Accept failed. cleanup and return error */
    
        /* Unlock the fd with error */
        fdint_unlockfd (pfd, error);
    
        llExit();
    
        return (INVALID_SOCKET);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function assigns a name to an unnamed socket. When a
     *      socket is created using "socket()" call, it exists in a
     *      name space (address family) but has no name assigned. The
     *      bind() function requests that name be assigned to the socket.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pName
     *     Handle to the sockaddr structure that holds the local
     *     address and port information that needs to be assigned to the
     *     socket.
     *
     *  @param[in]  len
     *     Holds the length of the sockaddr structure being passed as
     *     argument to this function. This in turn depends on the
     *     address family of the socket.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_bind( SOCKET s, struct sockaddr *pName, int len )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Validate Input */
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify Address Size */
        if (!pName || ((pName->sa_family == AF_INET) &&
            (len != sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
           || ((pName->sa_family == AF_INET6) &&
           (len != sizeof(struct sockaddr_in6)))
    #endif
          )
        {
            error = NDK_EINVAL;
            goto bind_error;
        }
    
        /* Bind the socket address */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if (error = Sock6Bind(pfd, pName))
                goto bind_error;
        }
        else
    #endif
        {
            if (error = SockBind(pfd, pName))
                goto bind_error;
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd(pfd, 0);
    
        llExit();
    
        return (0);
    
    bind_error:
        /* Check error condition */
    
        /* Unlock the fd with error */
        fdint_unlockfd(pfd, error);
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function establishes a logical connection from
     *      the socket specified by s to the foreign name (address)
     *      specified by pName.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pName
     *     Handle to the sockaddr structure that holds the remote host's
     *     address and port information to which the socket needs to connect to.
     *     For UDP/SOCK_DGRAM socket pName specifies the address to which
     *     packets would be sent by default or can be received from.
     *     For TCP/SOCK_STREAM socket this call attempts to make a connection
     *     to the socket that is bound to address specified by pName.
     *
     *  @param[in]  len
     *     Holds the length of the sockaddr structure being passed as
     *     argument to this function. This in turn depends on the
     *     address family of the socket.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_connect( SOCKET s, struct sockaddr *pName, int len )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Validate Input */
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify Address Size */
        if ((pName->sa_family == AF_INET && len != sizeof(struct sockaddr_in))
    #ifdef _INCLUDE_IPv6_CODE
           || (pName->sa_family == AF_INET6 && len != sizeof(struct sockaddr_in6))
    #endif
          )
        {
            error = NDK_EINVAL;
            goto connect_error;
        }
    
        /* Connect to the remote host */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if (error = Sock6Connect( pfd, pName ))
                goto connect_error;
        }
        else
    #endif
        {
            if (error = SockConnect( pfd, pName ))
                goto connect_error;
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return (0);
    
    connect_error:
        /* Error. Unlock the fd with error */
        fdint_unlockfd( pfd, error );
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      The getpeername() function retrieves the peer address of
     *      the specified socket, store this address in the sockaddr
     *      structure pointed to by the pName argument, and store the
     *      length of this address in plen argument.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[out]  pName
     *     Handle to the sockaddr structure that holds the remote host's
     *     address and port information to which the socket is connected to.
     *     Valid only when this function returns success.
     *
     *  @param[out]  plen
     *     Holds the length of the sockaddr structure being passed as
     *     result from this function. Valid only when this function returns
     *     success.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_getpeername( SOCKET s, struct sockaddr *pName, int *plen )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify Address Size */
        if (!pName || !plen || ((pName->sa_family == AF_INET) &&
            (*plen < (int)sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
            || ((pName->sa_family == AF_INET6) &&
            (*plen < (int)sizeof(struct sockaddr_in6)))
    #endif
          )
        {
            error = NDK_EINVAL;
            goto peername_error;
        }
    
        /* Get peer socket's name */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if (error = Sock6GetName(pfd, 0, pName))
                goto peername_error;
    
            /* Return Addr size when pointer is supplied */
            if (plen)
                *plen = sizeof(struct sockaddr_in6);
        }
        else
    #endif
        {
            if (error = SockGetName(pfd, 0, pName))
                goto peername_error;
    
            /* Return Addr size when pointer is supplied */
            if (plen)
                *plen = sizeof(struct sockaddr_in);
        }
    
        /* Unlock the fd without error */
        fdint_unlockfd(pfd, 0);
    
        llExit();
    
        return (0);
    
    peername_error:
        /* Unlock the fd with error */
        fdint_unlockfd(pfd, error);
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      The getsockname() function retrieves the local address of
     *      the specified socket, store this address in the sockaddr
     *      structure pointed to by the pName argument, and store the
     *      length of this address in plen argument.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[out]  pName
     *     Handle to the sockaddr structure that holds the local host's
     *     address and port information to which the socket is bound to.
     *     Valid only when this function returns success.
     *
     *  @param[out]  plen
     *     Holds the length of the sockaddr structure being passed as
     *     result from this function. Valid only when this function returns
     *     success.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_getsockname( SOCKET s, struct sockaddr *pName, int *plen )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify Address Size */
        if (!pName || !plen || ((pName->sa_family == AF_INET) &&
            (*plen < (int)sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
            || ((pName->sa_family == AF_INET6) &&
            (*plen < (int)sizeof(struct sockaddr_in6)))
    #endif
           )
        {
            error = NDK_EINVAL;
            goto sockname_error;
        }
    
        /* Get socket's name */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if(error = Sock6GetName(pfd, pName, 0))
                goto sockname_error;
    
            /* Return Addr size when pointer is supplied */
            if (plen)
                *plen = sizeof(struct sockaddr_in6);
        }
        else
    #endif
        {
            if(error = SockGetName(pfd, pName, 0))
                goto sockname_error;
    
            /* Return Addr size when pointer is supplied */
            if (plen)
                *plen = sizeof(struct sockaddr_in);
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return(0);
    
    sockname_error:
        /* getsockname() failed. Unlock the fd with error */
        fdint_unlockfd( pfd, error );
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function enables the socket to wait for any incoming
     *      connection requests. It also configures the size of the pending
     *      connection request queue of the socket. This call is applicable
     *      only for connection oriented sockets (SOCK_STREAM/TCP).
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  maxcon
     *      Specifies the maximum length of the queue of pending connections.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_listen( SOCKET s, int maxcon )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Listen */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if((error = Sock6Listen(pfd, maxcon)))
                goto listen_error;
        }
        else
    #endif
        {
            if((error = SockListen(pfd, maxcon)))
                goto listen_error;
        }
    
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return (0);
    
    listen_error:
        /* Unlock the fd with error */
        fdint_unlockfd(pfd, error);
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function is used to read data received on a
     *      specified socket.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pbuf
     *      Specifies the buffer to which the data has to be copied to.
     *
     *  @param[in]  size
     *      Specifies the maximum size of the buffer.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @retval
     *      Success -   Number of bytes of data received successfully
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_recv( SOCKET s, void *pbuf, int size, int flags )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        int32_t  rxsize;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 / PIPE / RAWETH */
        if ((fdint_lockfd(pfd, 0) == SOCKET_ERROR) )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Receive data  */
        if( pfd->Type == HTYPE_SOCK )
            error = SockRecv(pfd, pbuf, (int32_t)size, flags, 0, &rxsize);
    #ifdef _INCLUDE_IPv6_CODE
        else if( pfd->Type == HTYPE_SOCK6 )
            error = Sock6Recv(pfd, pbuf, (int32_t)size, flags, 0, &rxsize);
    #endif
        else if( pfd->Type == HTYPE_RAWETHSOCK )
        {
            /* For now, we only support no-copy version of recv on
             * raw ethernet sockets, so return error on recv().
             */
            error = NDK_EOPNOTSUPP;
        }
        else
            error = PipeRecv(pfd, pbuf, (int32_t)size, flags, &rxsize);
    
        if (error)
        {
            /* Unlock the fd with error */
            fdint_unlockfd( pfd, error );
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return ((int)rxsize);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function attempts to receive data from a socket. It is
     *      normally called with unconnected, non-connection oriented sockets.
     *      The data is placed into the buffer specified by pbuf, up to a maximum
     *      length specified by size. The options in flags can be used to change
     *      the default behavior of the operation. The name (address) of the sender
     *      is written to pName.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pbuf
     *      Specifies the buffer to which the data has to be copied to.
     *
     *  @param[in]  size
     *      Specifies the maximum size of the buffer.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @param[out] pName
     *      Pointer to place name (address) of sender
     *
     *  @param[out] plen
     *      Pointer to size of pName
     *
     *  @retval
     *      Success -   Number of bytes of data received successfully
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_recvfrom( SOCKET s, void *pbuf, int size, int flags, struct sockaddr *pName, int *plen )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        int32_t  rxsize;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
          )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Validate Sizes and Pointers */
        if (pName && (!plen || ((pName->sa_family == AF_INET) &&
            (*plen < (int)sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
            ||  ((pName->sa_family == AF_INET6) &&
            (*plen < (int)sizeof(struct sockaddr_in6)))
    #endif
           ))
        {
            error = NDK_EINVAL;
            goto recv_error;
        }
    
        /* Receive data - use Socket or Pipe send based on type */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if ((error = Sock6Recv(pfd, pbuf, (int32_t)size, flags, pName, &rxsize)))
                goto recv_error;
    
            /* Return Addr size */
            if (plen)
                *plen = sizeof(struct sockaddr_in6);
        }
        else
    #endif
        {
            if ((error = SockRecv(pfd, pbuf, (int32_t)size, flags, pName, &rxsize)))
                goto recv_error;
    
            /* Return Addr size */
            if (plen)
                *plen = sizeof(struct sockaddr_in);
        }
    
        /* Success. Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return ((int)rxsize);
    
    recv_error:
        /* Unlock the fd with error */
        fdint_unlockfd( pfd, error );
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *     This function attempts to send data on a socket. It is used on
     *     connected sockets only. The data to send is contained in the buffer
     *     specified by pbuf, with a length specified by size. The options in flags
     *     can be used to change the default behavior of the operation. The functions
     *     returns the length of the data transmitted on successful completion.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pbuf
     *     Data buffer holding data to transmit
     *
     *  @param[in]  size
     *     Size of data.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @retval
     *      Success -   Number of bytes of data sent successfully
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_send( SOCKET s, void *pbuf, int size, int flags )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        int32_t  txsize;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 / PIPE */
        if ((fdint_lockfd(pfd, 0) == SOCKET_ERROR) )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Send data */
        if (pfd->Type == HTYPE_SOCK)
        {
            error = SockSend(pfd, pbuf, (int32_t)size, flags, &txsize);
        }
    #ifdef _INCLUDE_IPv6_CODE
        else if (pfd->Type == HTYPE_SOCK6)
            error = Sock6Send(pfd, pbuf, (int32_t)size, flags, &txsize);
    #endif
        else if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            error = RawEthSockSend(pfd, pbuf, (int32_t)size, &txsize);
        }
        else
            error = PipeSend(pfd, pbuf, (int32_t)size, flags, &txsize);
    
        if (error)
        {
            /* Unlock the fd with error */
            fdint_unlockfd( pfd, error );
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return ((int)txsize);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function allocates bufSize bytes memory for the
     *      data buffer and required memory for the packet buffer to
     *      hold this data. On successful memory allocation, it
     *      initializes the phBuf and phPkt pointers with the data
     *      buffer and packet buffer handles. The data buffer obtained
     *      from this API can be used by the application to fill in
     *      required data. The application then would need to use the
     *      data buffer and packet buffer handles in its call to sendnc()
     *      API to send the packet out without any copy on transmit path
     *      by the stack. The packet and data buffers are freed up automatically
     *      once the packet transmission is completed in the ethernet driver.
     *      However, if for some reason the application would like to free
     *      the buffer and packet obtained using this call, it can to do so
     *      by passing the packet buffer handle to sendncfree() API call and it
     *      would free up both the packet and data buffers.
     *
     *      This API is currently only supported for AF_RAWETH family sockets.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  bufSize
     *     Size of data buffer to allocate memory for.
     *
     *  @param[in]  phBuf
     *     Pointer to data buffer handle in which the application can
     *     fill in the required data to send using sendnc() API.
     *
     * *  @param[in]  phPkt
     *     Pointer to the packet buffer handle which holds the data buffer
     *     in turn.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_getsendncbuff(SOCKET s, uint32_t bufSize, void** phBuf, void ** phPkt)
    {
        FILEDESC *pfd = (FILEDESC *)s;
        PBM_Pkt*    pPkt;
        uint32_t    error;
    
        llEnter();
    
        /* Lock the fd - type must be RAWETHSOCK */
        if (fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR)
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Allocate space for packet and data buffers. */
        pPkt = (void *)RawEthSockCreatePacket(pfd, bufSize, &error);
    
        /* Check if the operation succeeded */
        if( !pPkt )
        {
            /* Unlock the fd with error */
            fdint_unlockfd( pfd, error );
    
            llExit();
            return( SOCKET_ERROR );
        }
        else
        {
            /* Successfully obtained a packet. */
    
            *phBuf = (void *)(pPkt->pDataBuffer + pPkt->DataOffset);
    
            *phPkt = (void *)pPkt;
    
            /* Unlock the fd without error */
            fdint_unlockfd( pfd, 0 );
    
            llExit();
        }
    
        /* Return Success */
        return 0;
    }
    
    /**
     *  @b Description
     *  @n
     *     This function attempts to send data on a socket without copy. The data to
     *     send is contained in the buffer specified by pbuf, with a length
     *     specified by size. Also, a valid handle to the packet buffer hPkt needs to be specified.
     *     This packet handle and the buffer pointer should have been obtained from getsendncbuf() call
     *     before calling this API. The options in flags can be used to change the default
     *     behavior of the operation. The functions returns the length of the data
     *     transmitted on successful completion.
     *
     *     This API is currently only supported for AF_RAWETH family sockets.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pbuf
     *     Data buffer holding data to transmit
     *
     *  @param[in]  size
     *     Size of data.
     *
     *  @param[in]  hPkt
     *     packet handle obtained previously from getsendncbuf() call.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @retval
     *      Success -   Number of bytes of data sent successfully
     *  @retval
     *      Error   -   -1
     *
     */
    /* ARGSUSED */
    int NDK_sendnc( SOCKET s, void *pbuf, int size, void *hPkt, int flags )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        int32_t  txsize;
    
        llEnter();
    
        /* Lock the fd - type must be SOCKRAWETH */
        if ((fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR) )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Send data */
        if ((error = RawEthSockSendNC(pfd, pbuf, (int32_t)size, hPkt, &txsize)))
        {
            /* Unlock the fd with error */
            fdint_unlockfd( pfd, error );
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return ((int)txsize);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function is used to free data buffers obtained using
     *      getsendncbuff() calls. This is supported only for Raw ethernet socket /
     *      AF_RAWETH family sockets.
     *
     *  @param[in]  hFrag
     *      Handle to receive buffer to free.
     *
     *  @retval
     *      None
     */
    void NDK_sendncfree( void *hFrag )
    {
        llEnter();
        if( hFrag )
            PBM_free( (PBM_Handle)hFrag );
        llExit();
    }
    
    /**
     *  @b Description
     *  @n
     *      This function is used to read data received on a
     *      specified socket without copying. This is supported
     *      only on IPv4/AF_INET family and Raw ethernet/AF_RAWETH sockets.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[out]  ppbuf
     *      Pointer to receive data buffer pointer.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @param[out]  phFrag
     *      Pointer to receive buffer handle.
     *
     *  @retval
     *      Success -   Number of bytes of data received successfully
     *  @retval
     *      Error   -   -1
     *
     *      Returns 0 on connection oriented sockets where the connection
     *      has been closed by the peer (or socket shutdown for read)
     */
    int NDK_recvnc( SOCKET s, void **ppbuf, int flags, void **phFrag )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        PBM_Pkt  *pPkt;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK/RAWETHSOCK */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR) &&
            (fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Validate Sizes and Pointers */
        if( !ppbuf || !phFrag )
        {
            error = NDK_EINVAL;
            goto recvnc_error;
        }
    
        /* Receive the data */
        if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            if (error = RawEthSockRecvNC(pfd, &pPkt))
                goto recvnc_error;
        }
    	else if (error = SockRecvNC(pfd, flags, 0, &pPkt))
            goto recvnc_error;
    
        /* Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        /* Check size from return frag */
        if( pPkt && !pPkt->ValidLen )
        {
            PBM_free( pPkt );
            pPkt = 0;
        }
    
        /* Return the frag and buffer pointer */
        *phFrag = (void *)pPkt;
        if( pPkt )
        {
            /* Return pointer and length of data */
            *ppbuf = pPkt->pDataBuffer + pPkt->DataOffset;
            return ((int)pPkt->ValidLen);
        }
    
        return(0);
    
    recvnc_error:
        /* Unlock the fd with error */
        fdint_unlockfd( pfd, error );
    
        llExit();
        return( SOCKET_ERROR );
    }
    
    /**
     *  @b Description
     *  @n
     *      This function attempts to receive data from a socket. It is
     *      normally called with unconnected, non-connection oriented sockets.
     *      A pointer to data is returned in ppbuf. A system handle used to free
     *      the buffer is returned in phFrag. Both of these pointers must be
     *      valid. The name (address) of the sender is written to pName. This
     *      function is only valid for IPv4/AF_INET family sockets.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[out]  ppbuf
     *      Pointer to receive data buffer pointer.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @param[out] pName
     *      Pointer to place name (address) of sender
     *
     *  @param[out] plen
     *      Pointer to size of pName
     *
     *  @param[out]  phFrag
     *      Pointer to receive buffer handle.
     *
     *  @retval
     *      Success -   Number of bytes of data received successfully
     *  @retval
     *      Error   -   -1
     *
     *      Returns 0 on connection oriented sockets where the connection
     *      has been closed by the peer (or socket shutdown for read)
     */
    int NDK_recvncfrom( SOCKET s, void **ppbuf, int flags, struct sockaddr *pName, int *plen, void **phFrag )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        PBM_Pkt  *pPkt;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK */
        if((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Validate Sizes and Pointers */
        if( !ppbuf || !phFrag || !pName || !plen || (pName->sa_family == AF_INET &&
            *plen < (int)sizeof(struct sockaddr_in)))
        {
            error = NDK_EINVAL;
            goto recvnc_error;
        }
    
        /* Receive data - works only with socket type */
        if(error = SockRecvNC(pfd, flags, pName, &pPkt))
            goto recvnc_error;
    
        /* Return Addr size */
        if (plen)
            *plen = sizeof(struct sockaddr_in);
    
        /* Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        /* Check size from return frag */
        if( pPkt && !pPkt->ValidLen )
        {
            PBM_free( pPkt );
            pPkt = 0;
        }
    
        /* Return the frag and buffer pointer */
        *phFrag = (void *)pPkt;
    
        if( pPkt )
        {
            /* Return pointer and length of data */
            *ppbuf = pPkt->pDataBuffer + pPkt->DataOffset;
            return((int)pPkt->ValidLen);
        }
        return(0);
    
    recvnc_error:
        /* Unlock the fd with error */
        fdint_unlockfd( pfd, error );
    
        llExit();
    
        return( SOCKET_ERROR );
    }
    
    /**
     *  @b Description
     *  @n
     *      This function is used to free data buffers obtained using
     *      recvnc() or recvncfrom() calls. This is supported
     *      only IPv4/AF_INET family sockets.
     *
     *  @param[in]  hFrag
     *      Handle to receive buffer to free.
     *
     *  @retval
     *      None
     */
    void NDK_recvncfree( void *hFrag )
    {
        llEnter();
        if( hFrag )
            PBM_free( (PBM_Handle)hFrag );
        llExit();
    }
    
    /**
     *  @b Description
     *  @n
     *      This function attempts to send data on a socket to a specified
     *      destination. It is used on unconnected, non-connection oriented \
     *      sockets only. The data to send is contained in the buffer specified
     *      by pbuf, with a length specified by size. The options in flags can
     *      be used to change the default behavior of the operation.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in]  pbuf
     *     Data buffer holding data to transmit
     *
     *  @param[in]  size
     *     Size of data.
     *
     *  @param[in]  flags
     *      Options flags
     *
     *  @param[out] pName
     *      Pointer to name (address) of destination
     *
     *  @param[out] len
     *     size of pName
     *
     *  @retval
     *      Success -   Number of bytes of data sent successfully
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_sendto( SOCKET s, void *pbuf, int size, int flags, struct sockaddr *pName, int len )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
        int32_t  txsize;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR)
    #ifdef _INCLUDE_IPv6_CODE
           && (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR)
    #endif
           )
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify Address Size */
        if (((pfd->Type == HTYPE_SOCK) && len != sizeof(struct sockaddr_in))
    #ifdef _INCLUDE_IPv6_CODE
           || ((pfd->Type == HTYPE_SOCK6) && len != sizeof(struct sockaddr_in6))
    #endif
           )
        {
            error = NDK_EINVAL;
            goto sendto_error;
        }
    
        /* Connect */
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            if ((error = Sock6Connect(pfd, pName)))
                goto sendto_error;
    
            /* Send */
            error = Sock6Send(pfd, pbuf, (int32_t)size, flags, &txsize);
    
            /* Disconnect */
            Sock6Disconnect(pfd);
        }
        else
    #endif
        {
            if ((error = SockConnect(pfd, pName)))
                goto sendto_error;
    
            /* Send */
            error = SockSend(pfd, pbuf, (int32_t)size, flags, &txsize);
    
            /* Disconnect */
            SockDisconnect(pfd);
        }
    
        /* Record any error condition */
        if (error)
            goto sendto_error;
    
        /* Unlock the fd without error */
        fdint_unlockfd(pfd, 0);
    
        llExit();
    
        return ((int)txsize);
    
    sendto_error:
        /* Unlock the fd with error */
        fdint_unlockfd(pfd, error);
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function causes all or part of a full-duplex
     *      connection on the socket associated with a socket to be shut down.
     *      If how is SHUT_RD (0), further receives will be disallowed.
     *      If how is SHUT_WR (1), further sends will be disallowed. If how is
     *      SHUT_RDWR (2), further sends and receives will be disallowed.
     *
     *  @param[in]  s
     *      Handle to a socket obtained using "socket" function call.
     *
     *  @param[in] how
     *      Manner of shutdown.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_shutdown( SOCKET s, int how )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK / SOCK6 */
        if ((fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR) &&
    #ifdef _INCLUDE_IPv6_CODE
           (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR) &&
    #endif
           (fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Shutdown the socket */
        if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            error = RawEthSockShutdown(pfd, how);
        }
        else
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            error = Sock6Shutdown(pfd, how);
        }
        else
    #endif
        {
            error = SockShutdown(pfd, how);
        }
    
        /* Check error condition */
        if (error)
        {
            /* Unlock the fd with error */
            fdint_unlockfd( pfd, error );
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return (0);
    }
    
    /**
     *  @b Description
     *  @n
     *      This function creates a socket, an endpoint for
     *      communication and returns the socket in the form
     *      of a file descriptor.
     *
     *  @param[in]  domain
     *      Socket domain/family. Valid values are AF_INET/AF_INET6.
     *
     *  @param[in] type
     *      Socket type (SOCK_DGRAM, SOCK_STREAM, SOCK_RAW).
     *
     *  @param[in] protocol
     *      Socket protocol (Normally IPPROTO_TCP or IPPROTO_UDP, but
     *      can be anything when type is set to SOCK_RAW)
     *
     *  @retval
     *      Success -   socket handle
     *  @retval
     *      Error   -   INVALID_SOCKET
     *
     */
    SOCKET NDK_socket( int domain, int type, int protocol )
    {
        FDTABLE  *pfdt;
        FILEDESC *pfd;
        int      error = 0;
    
        llEnter();
    
        /* Verify Socket Session */
        if (!fdint_getfdt(0))
        {
            llExit();
            return( INVALID_SOCKET );
        }
    
    #ifdef _INCLUDE_IPv6_CODE
        if (domain == AF_INET6)
        {
            /* Create a new IPv6 socket */
            if ((error=Sock6New(domain, type, protocol, 0, 0, (void **)&pfd)))
                goto socket_error;
        }
        else
    #endif
        if (domain == AF_INET)
        {
            /* Create a new IPv4 socket */
            if((error=SockNew(domain, type, protocol, 0, 0, (void **)&pfd)))
                goto socket_error;
        }
        else if (domain == AF_RAWETH)
        {
            /* Create a new Raw Ethernet socket */
            if((error=RawEthSockNew(domain, type, protocol, 0, 0, (void **)&pfd)))
                goto socket_error;
        }
        else
        {
            /* Unknown Protocol Family type. Only Supported Families are:
             * AF_INET/AF_INET6/AF_RAWETH.
             */
            error = NDK_EPFNOSUPPORT;
            goto socket_error;
        }
    
    
        /* Success. Return the file descriptor table index */
        llExit();
    
        return (pfd);
    
    socket_error:
        if (((pfdt=fdint_getfdt(0)) != 0))
            pfdt->error = error;
    
        llExit();
    
        return (INVALID_SOCKET);
    }
    
    /**
     *  @b Description
     *  @n
     *     This function returns the options associated with a
     *     socket.
     *
     *  @param[in]  s
     *      Socket handle
     *
     *  @param[in] level
     *      Option level (SOL_SOCKET, IPPROTO_IP, IPPROTO_IPV6,IPPROTO_TCP)
     *
     *  @param[in] op
     *      Socket option to get
     *
     *  @param[in] pbuf
     *      Pointer to memory buffer
     *
     *  @param[in] pbufsize
     *      Pointer to size of memory buffer
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_getsockopt( SOCKET s, int level, int op, void *pbuf, int *pbufsize )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK/SOCK6 */
        if (fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR &&
    #ifdef _INCLUDE_IPv6_CODE
           (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR) &&
    #endif
           (fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Get Option */
        if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            error = RawEthSockGet(pfd, level, op, pbuf, pbufsize);
        }
        else
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            error = Sock6Get(pfd, level, op, pbuf, pbufsize);
        }
        else
    #endif
        {
            error = SockGet(pfd, level, op, pbuf, pbufsize);
        }
    
        /* Check error condition */
        if (error)
        {
            /* Unlock the fd with error */
            fdint_unlockfd(pfd, error);
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Success.Unlock the fd without error */
        fdint_unlockfd( pfd, 0 );
    
        llExit();
    
        return (0);
    }
    
    /**
     *  @b Description
     *  @n
     *     This function sets the option values associated with a
     *     socket.
     *
     *  @param[in]  s
     *      Socket handle
     *
     *  @param[in] level
     *      Option level (SOL_SOCKET, IPPROTO_IP, IPPROTO_IPV6,IPPROTO_TCP)
     *
     *  @param[in] op
     *      Socket option to set
     *
     *  @param[in] pbuf
     *      Pointer to memory buffer
     *
     *  @param[in] bufsize
     *      Size of memory buffer pointed to by pbuf
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_setsockopt( SOCKET s, int level, int op, void *pbuf, int bufsize )
    {
        FILEDESC *pfd = (FILEDESC *)s;
        int  error = 0;
    
        llEnter();
    
        /* Lock the fd - type must be SOCK/SOCK6 */
        if (fdint_lockfd(pfd, HTYPE_SOCK) == SOCKET_ERROR &&
    #ifdef _INCLUDE_IPv6_CODE
           (fdint_lockfd(pfd, HTYPE_SOCK6) == SOCKET_ERROR) &&
    #endif
           (fdint_lockfd(pfd, HTYPE_RAWETHSOCK) == SOCKET_ERROR))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Set Option */
        if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            error = RawEthSockSet(pfd, level, op, pbuf, bufsize);
        }
        else
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            error = Sock6Set(pfd, level, op, pbuf, bufsize);
        }
        else
    #endif
        {
            error = SockSet(pfd, level, op, pbuf, bufsize);
        }
    
        /* Check error condition */
        if (error)
        {
            /* Unlock the fd with error */
            fdint_unlockfd(pfd, error);
    
            llExit();
    
            return (SOCKET_ERROR);
        }
    
        /* Unlock the fd without error */
        fdint_unlockfd(pfd, 0);
    
        llExit();
    
        return (0);
    }
    
    /**
     *  @b Description
     *  @n
     *      Creates a pre-connected full duplex pipe. The returned file
     *      descriptors can be used with all the fd file descriptor functions,
     *      as well as the send() and recv() socket functions.
     *
     *  @param[in]  pfdret1
     *      Pointer to file descriptor to first end of pipe.
     *
     *  @param[in] pfdret2
     *      Pointer to file descriptor to second end of pipe.
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_pipe( void **pfdret1, void **pfdret2 )
    {
        FDTABLE  *pfdt;
        FILEDESC *pfd1=0,*pfd2=0;
        int      error = 0;
    
        llEnter();
    
        /* Verify Socket Session */
        if (!fdint_getfdt(0))
        {
            llExit();
            return( SOCKET_ERROR );
        }
    
        /* Verify the fd pointers */
        if (!pfdret1 || !pfdret2)
        {
            error = NDK_EINVAL;
            goto pipe_error;
        }
    
        /* Create a new pipe */
        if ((error=PipeNew( (void **)&pfd1, (void **)&pfd2 )))
            goto pipe_error;
    
        llExit();
    
        /* Return the file descriptor table indicies */
        *pfdret1 = pfd1;
        *pfdret2 = pfd2;
    
        return (0);
    
    pipe_error:
        if ((pfdt=fdint_getfdt(0)) != 0)
            pfdt->error = error;
    
        llExit();
    
        return (SOCKET_ERROR);
    }
    
    /**
     *  @b Description
     *  @n
     *      Get a sockets context value. When using the slnetifndk libary the
     *      context will be the index of the socket in the slnetifndk socket table.
     *
     *  @param[in]  s
     *      Socket to get context from
     *
     *  @retval
     *      Success -   context number
     *  @retval
     *      Error   -   -1
     *
     */
    int NDK_getSockCtx( SOCKET s)
    {
        int context;
        FILEDESC *pfd = (FILEDESC *)s;
    
        if( s == NULL)
        {
            return (-1);
        }
    
        if (pfd->Type == HTYPE_RAWETHSOCK)
        {
            context = RawEthSockGetCtx(s);
        }
        else
    #ifdef _INCLUDE_IPv6_CODE
        if (pfd->Type == HTYPE_SOCK6)
        {
            context = Sock6GetCtx(s);
        }
        else
    #endif
        {
            context = SockGetCtx(s);
        }
    
        return (context);
    }
    
    /**
     *  @b Description
     *  @n
     *      Registers a NDK_HookFxn of a given type. For instance a
     *      CREATE_SKT_CTX_HOOK type will register the function inside SockNew
     *
     *  @param[in]  type
     *      NDK_HookFxn function type.
     *
     *  @param[in]  fxn
     *      The NDK_HookFxn to register.
     *
     *  @retval
     *      None
     */
    void NDK_registerHook(int type, NDK_HookFxn fxn) {
        switch(type) {
            case CREATE_SKT_CTX_HOOK:
                NDK_createSockCtx = fxn;
                break;
            case CLOSE_SKT_CTX_HOOK:
                NDK_closeSockCtx = fxn;
                break;
            case NETSTART_ERROR_HOOK:
                NDK_netStartError = fxn;
                break;
            default:
                break;
        }
    }
    

    0336.slnetifndk.c

    Regards,
    Pavel

  • Hi Pavel,

    thanks for the files.

    Yes, v3.60.00.13 still contains the issue I'm talking about:

    NDK_accept() in socket.c still contains the check mentioned above at line 116/119:

        /* If there's a name, there must be a valid length */
        /*
         * Note64: sizeof returns size_t, which is 64 bit unsigned for
         * LP64. May need to cast to int32_t to avoid implicit type conversions
         */
        if (pName && (!plen || ((pName->sa_family == AF_INET) &&
            (*plen < (int)sizeof(struct sockaddr_in)))
    #ifdef _INCLUDE_IPv6_CODE
            || ((pName->sa_family == AF_INET6) &&
            (*plen < (int)sizeof(struct sockaddr_in6)))
    #endif
           ))
        {
            error = NDK_EINVAL;
            goto accept_error;
        }
    

    spru524k clearly says:

    "The argument pName is a result parameter that is filled in with the address of the connecting entity as known to the communications layer." (Chapter 3.3.3, page 48). It doesn't mention that pName->sa_family must be provided properly!

    So IMHO definitely code and documentation do not match. I'd suggest to change code as stated in my first message (pfd->Type == HTYPE_SOCK / pfd->Type == HTYPE_SOCK6) as this is the check used later on at line 166 to decide if pName should be treated as struct sockaddr_in or struct sockaddr_in6.

    Best regards,
    Lars

  • Hi Lars,

    Thanks for bringing this to our attention, I looked into it and it looks like an actual bug in the NDK. I have filed this bug internally, it is tracked by: NDK-452

    Regards,
    Gerardo

  • Hi Gerardo,

    thanks for accepting the issue. :-)

    Best regards,
    Lars