This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

コンパイラ/ TMS320C6747: Should I change the BIOS version?

Part Number: TMS320C6747

Tool/software: TI C / C ++コンパイラ

Hello Mr. Rahul

I was able to grasp the important part with your help.
Among the sources of development results nine years ago, I will send a tcf file with attribute txt. Development target is a custom board. tcf is the bios config file, isn't it? Do you see this and do you know the BIOS version? I feel like I have to match the BIOS with this when enhancing this time, but how is it?Or is it better to match the platform to bios?
By the way, the tools used at that time are as follows.
TMDSCCS-ALLN01-v4.0 (Code Composer Studio IDE V4)
 DSPBIOS5_41_03_17
 C6747_BIOSPSP_01_30_01
 EDMA3_LLD_BIOS5_01_11_00_03
XDS510 USB (JTAG EMULATOR)

Best Regards

Suzuki

utils.loadPlatform("myplatforms.C6747_LS041");

/* The following DSP/BIOS Features are enabled.  */
bios.enableRealTimeAnalysis(prog);
bios.enableRtdx(prog);
bios.enableTskManager(prog);

bios.GBL.CLKIN = 24000;
bios.GBL.C64PLUSMAR128to159 = 0x0000ffff;
bios.MEM.instance("L3_CBA_RAM").space = "data";
bios.MBX.create("Mbx_fcnt");
bios.MBX.instance("Mbx_fcnt").comment = "Fcnt_tsk mailbox";
bios.MBX.instance("Mbx_fcnt").messageSize = 4;
bios.TSK.instance("TSK_idle").order = 1;
bios.TSK.create("TSK_cmd");
bios.TSK.instance("TSK_cmd").order = 1;
bios.TSK.instance("TSK_cmd").comment = "Cmd_tsk";
bios.TSK.instance("TSK_cmd").fxn = prog.extern("Cmd_tsk");
bios.TSK.create("TSK_fcnt");
bios.TSK.instance("TSK_fcnt").order = 2;
bios.TSK.instance("TSK_fcnt").comment = "Fcnt_tsk";
bios.TSK.instance("TSK_fcnt").fxn = prog.extern("Fcnt_tsk");
bios.GBL.CALLUSERINITFXN = 1;
bios.GBL.USERINITFXN = prog.extern("Psc_init");
bios.ECM.ENABLE = 1;
bios.HWI.instance("HWI_INT7").interruptSelectNumber = 0;
bios.HWI.instance("HWI_INT8").interruptSelectNumber = 1;
bios.HWI.instance("HWI_INT9").interruptSelectNumber = 2;
bios.HWI.instance("HWI_INT10").interruptSelectNumber = 3;
bios.MBX.create("Mbx_acf");
bios.MBX.instance("Mbx_acf").messageSize = 4;
bios.TSK.create("TSK_acf");
bios.TSK.instance("TSK_acf").order = 3;
bios.TSK.instance("TSK_acf").comment = "Acf_tsk";
bios.TSK.instance("TSK_acf").fxn = prog.extern("Acf_tsk");
bios.TSK.create("TSK_led");
bios.TSK.instance("TSK_led").order = 4;
bios.TSK.instance("TSK_led").comment = "Led_tsk";
bios.TSK.instance("TSK_led").fxn = prog.extern("Led_tsk");
bios.TSK.create("TSK_tx");
bios.TSK.instance("TSK_tx").order = 5;
bios.TSK.instance("TSK_tx").comment = "Tx_tsk";
bios.TSK.instance("TSK_tx").fxn = prog.extern("Tx_tsk");
bios.UDEV.create("UART0");
bios.UDEV.instance("UART0").comment = "UART0";
bios.UDEV.instance("UART0").initFxn = prog.extern("user_uart0_init");
bios.UDEV.instance("UART0").fxnTable = prog.extern("uartParams", "asm");
bios.UDEV.instance("UART0").fxnTableType = "IOM_Fxns";
bios.UDEV.instance("UART0").fxnTable = prog.extern("Uart_IOMFXNS");
bios.UDEV.instance("UART0").params = prog.extern("uartParams");
bios.MEM.instance("IRAM").base = 0x11800400;
bios.MEM.instance("IRAM").len = 0x0003fc00;
bios.MEM.create("BOOT");
bios.MEM.instance("BOOT").comment = "BOOT LOADER";
bios.MEM.instance("BOOT").base = 0x11800000;
bios.MEM.instance("BOOT").len = 0x00000400;
bios.MEM.instance("BOOT").space = "code/data";
bios.MEM.STACKSIZE = 0x2000;
bios.RTDX.MODE = "Simulator";
bios.MEM.NOMEMORYHEAPS = 0;
bios.MEM.instance("IRAM").createHeap = 1;
bios.MEM.instance("IRAM").heapSize = 0x00004000;
bios.MEM.BIOSOBJSEG = prog.get("IRAM");
bios.MEM.MALLOCSEG = prog.get("IRAM");
bios.LOG.create("TRACE");
bios.LOG.instance("TRACE").bufLen = 512;
bios.MEM.create("FROM");
bios.MEM.instance("FROM").createHeap = 0;
bios.MEM.instance("FROM").space = "reserved";
bios.MEM.instance("FROM").comment = "FLASH ROM";
bios.MEM.instance("FROM").base = 0x60000000;
bios.MEM.instance("FROM").len = 0x00200000;
bios.GIO.ENABLEGIO = 1;
bios.TSK.instance("TSK_fcnt").stackSize = 4096;
bios.RTDX.MODE = "JTAG";
bios.SEM.create("Sem_Acf_data");
bios.SEM.instance("Sem_Acf_data").count = 1;
bios.TSK.instance("TSK_acf").priority = 2;
bios.TSK.instance("TSK_fcnt").priority = 2;
bios.TSK.instance("TSK_led").priority = 2;
bios.TSK.instance("TSK_cmd").order = 2;
bios.TSK.instance("TSK_fcnt").order = 3;
bios.TSK.instance("TSK_acf").order = 4;
bios.TSK.instance("TSK_led").order = 5;
bios.TSK.instance("TSK_tx").destroy();
bios.MEM.instance("BOOT").len = 0x00004000;
bios.MEM.instance("IRAM").base = 0x11804000;
bios.MEM.instance("IRAM").len = 0x0003c000;
bios.LOG.instance("TRACE").destroy();
bios.MEM.instance("BOOT").len = 0x00000800;
bios.MEM.instance("IRAM").base = 0x11800800;
bios.MEM.instance("IRAM").len = 0x0003f800;
bios.TSK.instance("TSK_acf").stackSize = 2048;
bios.TSK.instance("TSK_cmd").stackSize = 8192;
bios.TSK.instance("TSK_led").stackSize = 2048;
bios.TSK.instance("TSK_idle").stackSize = 2048;
bios.UDEV.instance("UART0").deviceId = 2;
bios.UDEV.instance("UART0").deviceId = 1;
bios.MEM.STACKSIZE = 0x4000;
bios.MEM.STACKSIZE = 0x2000;
bios.UDEV.instance("UART0").deviceId = 0;
bios.UDEV.instance("UART0").deviceId = 2;
bios.UDEV.instance("UART0").deviceId = 0;
// !GRAPHICAL_CONFIG_TOOL_SCRIPT_INSERT_POINT!

prog.gen();

  • Hi,

    tcf is the bios config file, isn't it?

    Yes, this is the config file for the outdated dsp bios versions. Latest SYS/BIOS use .cfg files.

    Do you see this and do you know the BIOS version?

    There is no way to tell the DSP BIOS version from the attached file, you should know which bios version you've used when creating the CCS Project. Also it shouldn't matter if you have set the correct values in the config file (.tcf)/

    Best Regards,
    Yordan

  • Yes, when working with 9 year old software to avoid incompatibilities, we recommend that you match the dependent components as much as possible. BAsed on the dependencies of C6747 BIOS PSP, the DSP BIOS version appears to be correct :

    Release Notes: http://software-dl.ti.com/dsps/dsps_public_sw/psp/BIOSPSP/01_30_01/content/C6747_BIOSPSP_ReleaseNotes.pdf

    In addition to DSP BIOS tcf file, the project also expects that the build provides the platform memory layout and default DSP settings using a platform definition. The default memory layout and DSP settings comes from the BIOS package but if a custom platform requires memory to be partitioned differently or doesn`t have the same memory size as the TI evaluation platform then BIOS provides users to provide a custom platform definition.

    If a user creates custom platform, they need to maintain this as part of their code base as TI will only provide platform definitions for HW evaluation platforms that we support.

    Regards,

    Rahul

  • Thank you Mr. Yordan
    I examined your information and decided to retry with ccsv4. The results aren't going well, so I'll write it together for Raffle. Please have a look there.

    Best Regards, 

    suzuki