Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: UNIFLASH
Hello -
I am trying to connect to a beagle bone black that has been extended and because of that it has no sd card. trying to connect via uart ideally to download the bootloader and ultimately the linux kernel . ethernet or usb would be fine as well. even jtag.. I am assuming I should be able to download what ever is current on a freshly installed ubuntu version with the current linux-processor-sdk and be able to build uboot and get the system loaded onto a beaglebone black. Apparently not. I have googled and downloaded and built and have had blockages in every part. I think the problem is that I cannot seem to find a current set of versions that work together to do this job. I wonder if there is a CURRENT description of exactly what tools to use and where to find them to do this pretty fundamental thing. I have beaglebone black and the basic evm . I have the latest ccs version (9.x.x). It is not clear which linaro version to use for compiling any of it. Is there a clear path that most people use? Uniflash looks pretty good but I cant even find the processor in the list. Is is a mistake to think the sitara am335x has support ? Can someone please point me in the right direction? Any advice on the easiest and quickest approach would be valuable as well.
Thanks
Mark