This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: DDR configuration

Part Number: AM5728

Hello,

We made a board and we did not use DDR (D2516EC4BXGGB, Kingston) used in AM572x Evaluation Module (TMDSEVM572X).

Instead, mt41k256m16tw-107 (Mircon) was used.
I used four 4Gbs just like the EVM board.

When I connect JTEG and check the Memory Browser, the data of some addresses is constantly changing.

When DDR changes, I wonder if the gel file needs to change.
The gel file I'm currently using is the default gel file (ccsv7 \ ccs_base \ emulation \ boards \ am572x \ gel)

How can I solve it?
I would appreciate it if you could tell me how.

If I need to change the gel file, I would like to attach the mt41k256m16tw-107 (Mircon) gel file for AM5728.

I am currently using without OS.

please answer me.
Thank you.